Sealing Shielding

Omega Profile: A More Robust PSA Backed Sealing Solution

Robust Sealing Solutions to Replace PSA Backed Seals, O-Ring & Engineered Seals Division, Hollow D sealCustomers often call with various sealing challenges. But sometimes their dilemmas can be solved with more robust solutions instead of direct replacements. For example, when a customer is having issues with a PSA-backed hollow seal that keeps peeling away from the bottom surface. 

If you need to seal a box with a lid, you may need a 4-corner gasket to seal the contents from dirt and moisture. If you use a solid gasket, the compression force may be too great to effectively close the lid. Using a hollow seal reduces the compression force by orders of magnitude, but it comes with its own set of challenges.

A hollow seal for a box will most often seal between two flat surfaces. The bottom surface will be flat for adhesion to the box, while the top surface is curved to engage the lid as it is seated on top of the seal. However, the disadvantage of this design is the tendency of the flat portion to lift off the bottom surface. Figure 1 illustrates this phenomenon with standard Parfab profile D015.

 

Robust Sealing Solutions to Replace PSA Backed Seals, O-Ring & Engineered Seals Division, Hollow D Profile D015 with 25 Percent Compression

 

 

 

 

 

 

 

 

 

 

 

Figure 1.  Hollow-D profile D015 with 25 percent compression.

In the analysis shown in Figure 1, the bowing is 0.030 inch at its highest point. Due to this tendency to bow upward, it is necessary to use Pressure Sensitive Adhesive (PSA) backing to keep the bottom surface in place during compression. However, due to the bowing of this surface, this stresses the PSA backing every time the seal is compressed. This can cause the PSA backing to eventually peel away. When this happens, the seal can also leak due to lack of seal contact on the bottom surface.

To address this issue, Parker offers the Omega seal profile, which has a hump in the middle of the flat portion to reduce bowing as the seal is compressed.Robust Sealing Solutions to Replace PSA Backed Seals, O-Ring & Engineered Seals Division, Omega seal

Figure 2 shows Omega seal profile W034. Like the D015 profile, it is also 0.500 inch high and is compressed 25 percent.

 

Robust Sealing Solutions to Replace PSA Backed Seals, O-Ring & Engineered Seals Division, Omega Seal Profile W034 with 25 Percent Compression

 

 

 

 

 

 

 

 

 

 

 

 

Figure 2.  Omega seal profile W034 with 25 percent compression.

As shown in Figure 2, the bowing of the bottom surface has been reduced from 0.030 inches to 0.004 inch, which greatly reduces peeling stress when PSA backing is used.

Figure 3 illustrates the standard profiles that we offer for the Omega seal profile.

Robust Sealing Solutions to Replace PSA Backed Seals, O-Ring & Engineered Seals Division, Parker Omega Part Number Configuration Table

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Figure 3.  Standard Omega seal profiles.

They are also available in a variety of different materials. They can be extruded as cord stock, or supplied as spliced four-corner gaskets for your particular lid or door sealing application.

For more information, visit Parker O-Ring & Engineered Seals Division online and chat with our experienced applications engineers.

 

 

Robust Sealing Solutions to Replace PSA Backed Seals, O-Ring & Engineered Seals Division, David Mahlbacher

 

 

This article was contributed by David Mahlbacher, Parker O-Ring & Engineered Seals Division, product design engineer for general industrial/consumer/onshore oil & gas. 

 

 

 

 

 

Related content:

Rapid Prototype Program Reduces Seal Project Lead Time

Environmental Seal Enclosure 101

Press-in-Place Seals for Axial Sealing Applications

Sealing Groove-less Applications with Flat Panel Gaskets

 

 

 

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Omega Profile: A More Robust PSA Backed Sealing Solution


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha