Considering that more than six million people live in the Philadelphia region, government officials realized they needed a fast-response emergency river vessel with both fire fighting and rescue capabilities for any type of emergency it may encounter. Philadelphia officials turned to Derecktor Shipyards, New York, to manufacture the Independence, a 2000-Class Fireboat, which was christened in December 2007.
Established in 1947, Derecktor Shipyards builds a variety of commercial vessels and custom mega yachts for customers around the world. The waterways around the Philadelphia region pose a significant and serious set of obstacles that needed to be considered when designing and building the Independence. With regional responsibilities from as far north as Trenton, New Jersey, and as far south as the Delaware Bay, the Independence would find itself in water depths as shallow as 30 inches. Furthermore, some of the waterways are very narrow, so the Independence was designed to make 360° turns.
The Independence is powered by four 825 horsepower engines, allowing it to achieve speeds of 36 knots. Its fire-fighting arsenal includes a water pump capable of 5500 gallons per minute and 200 foam tank capacity. It also has a 16-ft rescue boat, and its galley can be converted into a trauma unit complete with advanced life support equipment.
However, the greatest challenge for the fireboat was its height. Many bridge structures in the area only allow vessels with an air draft of 18 feet to pass underneath. Air draft is the distance from the water surface to the upper-most point of a vessel. Therefore. keeping the air draft of the Independence less than 18 feet was imperative to its safe travel and access to all areas within its range.
To enable the Independence to achieve an air draft of only 18 feet, a navigation tower on top of the pilothouse needed to be pivoted 110°. This is accomplished using a helical rotary actuator from Parker’s Cylinder Division.

According to Joe Beckham, project manager at Derecktor Shipyards. “With the navigation mast situated on top of the pilothouse, determining how to rotate it through its 110° of travel was difficult." Hydraulic cylinders and electromechanical positioning devices had been considered, but a Helac L20-15-E-FT-180 rotary actuator was specified to position the mast.
Helac actuators are designed to replace multiple components and function as a rotating device, mounting bracket, and bearing, all-in-one. The innovative, sliding-spline operation technology of a Helac actuator converts linear piston motion into powerful shaft rotation. Each actuator is composed of a housing and two moving parts — the central shaft and piston. Helical spline teeth on the shaft engage matching teeth on the piston’s inside diameter. The second set of helical splines on the piston’s outside diameter mesh with the gear in the housing.
Beckham summarized the rationale of partnering with Parker in four major points. First, the Helac rotary actuator makes better use of space than the other alternative considered. Hydraulic cylinders and electromechanical positioning devices would have required a well or cavity below the mast. This well would have protruded down into the pilothouse. Considering the limited space available, the compact design of the rotary actuator made it the optimal choice.
Second, the Helac rotary actuator requires less maintenance as a positioning device than hydraulic cylinders. Sealing occurs against smooth cylindrical surfaces, effectively eliminating all leakage and holding selected positions without drift. There are no external moving parts, which eliminates the service and maintenance issues often associated with hydraulic cylinders and mechanical linkages in a marine application.
Third, this helical rotary actuator delivers high torque and 110° of smooth rotation from the limited hydraulic supply with power to spare. Achieving 110° of rotation is possible with alternative solutions. However, the L20-15 delivers up to 15,000 pounds per inch of torque and produces consistent, smooth motion from a 3,000 psi hydraulic source.
Fourth, Derecktor shipyards saved substantial installation time and cost because the L20-15 serves the double function of the rotary actuator and bearing support all in one compact package. This self-contained design reduced the number of parts required of the mast assembly.

This article was contributed by Jessica Howisey, marketing communications manager and Daniel Morgado, applications engineer, Helac Business Unit, Cylinder Division and was originally published by Hydraulics & Pneumatics
Related articles:
Know Your Pneumatics: Rotary Actuator Basics
Know Your Pneumatics: Which Rotary Actuator Should I Choose?
Lifters Designed with Rotary Actuators Dump Waste More Effectively
Have a question about Parker products or services? We can help: Contact Us!
Comments for Rotary Actuator Lowers Fire Boat to Fit Under Bridges
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.