There is growing, perhaps booming, commercial investment in
electric vertical takeoff and landing (eVTOL) vehicles that will
serve the new urban air mobility (UAM) aerospace market. Upstart
and...
Posted On 01/22/2021
Read More ►
Hydraulic fluid particle detection is essential in maintaining the
performance of the systems and equipment requiring the movement of
materials and parts. Standard operating procedures call for...
Posted On 01/19/2021
Read More ►
Small and mid-scale LNG plants are dramatically changing the
application sphere for natural gas as an alternative fuel for
transportation, both onland and for marine shipping use. They are
helping...
Posted On 01/14/2021
Read More ►
In the quest for a decarbonised society there is no doubt that
Hydrogen as an environmentally friendly fuel source is gaining a
lot of popularity to become the fuel of the future. And the
hydrogen...
Posted On 12/16/2020
Read More ►
Forklift manufacturers need to be focused on building equipment
that is reliable, durable and designed for safety. The forklift’s
mast, or upright, is the portion of the forklift that lifts,...
Posted On 12/15/2020
Read More ►
If your dust is combustible, you need to be concerned with the
risk. According to a report published by Dust Safety Science¹, 34
dust explosions and 115 fires were logged globally in just the
first...
Posted On 12/09/2020
Read More ►
It’s a sobering fact that many of the support structures holding up
the world’s electrical grid are nearing the end of their
serviceable life. After 50 or so years, wooden electric poles
and...
Posted On 12/08/2020
Read More ►
Wind turbines are designed to maximize power production based on
the predicted wind speeds found at the plant site. However,
excessive wind speeds are experienced at times, so it is crucial to
limit...
Posted On 11/24/2020
Read More ►
ZoomLock MAX press-to-connect flame-free refrigerant fittings help
to improve productivity for HVACR contractors and technicians on
the job. Having the ZoomLock MAX complete system equipped with...
Posted On 10/08/2020
Read More ►
As production facilities managers can attest, global wine
production and consumption continue to flourish. Record
production levels of 293 million hectolitre were reached during
2018. Europe continues...
Posted On 10/08/2020
Read More ►
As advanced manufacturing factories gain importance, manufacturers
must prioritize what benefits and supporting programs will prepare
their factories to best meet the evolving needs of their...
Posted On 09/24/2020
Read More ►
The food and beverage industry is the largest manufacturing sector
to use chilled water systems. Applications within the industry are
very diverse due to the wide range of product types and how...
Posted On 09/17/2020
Read More ►
The safe navigation of ships in challenging marine environments is
a testament to the skill of the crew and the performance of the
equipment they use. In offshore applications, the ambient
environment...
Posted On 09/16/2020
Read More ►
Parker Sporlan’s ZoomLock MAX press-to-connect refrigerant
fittings, designed for the air conditioning and refrigeration
markets, allows HVACR contractors to make secure leak-free
connections in...
Posted On 09/16/2020
Read More ►
Improving indoor air quality (IAQ) has been a major focus in
manufacturing, industrial, and other commercial environments for
decades, given that poor IAQ can not only cause immediate
deleterious...
Posted On 09/08/2020
Read More ►
For today’s industrial pneumatic systems, automation and efficiency
continue to be the driving factors in design. Automation in
pneumatics incorporates a variety of design strategies...
Posted On 06/30/2020
Read More ►
In the manufacturing sector, anywhere that humans mix with
machinery is a potential danger zone. Even in the modern
production line, people are often still an essential element of the
production or...
Posted On 06/17/2020
Read More ►
Human error in bioprocessing can have serious consequences for
biopharmaceutical manufacturers. Accidents can cause a health
hazard for staff involved in bioprocessing operations and human
error can...
Posted On 06/09/2020
Read More ►
The high transmission rate of coronavirus (COVID-19) has prompted
the Center for Disease Control and Prevention (CDC) to recommend
that everyone in the U.S. wear nonsurgical face masks when going
out...
Posted On 06/04/2020
Read More ►
Looking ahead to the future of industry, with all the advancements
in technology that the Industrial Internet of Things (IIoT) holds
in store, one might rightly wonder if pneumatics will still...
Posted On 06/04/2020
Read More ►