Thermal interface materials are used to eliminate air gaps or voids
from adjoining rough or un-even mating surfaces. Because the
thermal interface material has a greater thermal conductivity than
the...
Posted On 01/11/2021
Read More ►
In 1933, Kenworth Motor Truck Co. became the first American truck
manufacturer to introduce the Cummins 4 cylinder, 100 hp, HA4 model
diesel engine as standard equipment. By 1938 the first...
Posted On 01/08/2021
Read More ►
Clean energy consultancy Gladstein, Neandross and Associates, in
its recent report on sustainable fleets¹, predicts another decade
of diesel-powered heavy trucks leading long-haul. Diesel...
Posted On 01/07/2021
Read More ►
While 2020 is notable for many events, for most of us, it was
an unprecedented period of change. Change in how (and where) we
work, conduct our daily activities, interact with colleagues,
family,...
Posted On 01/07/2021
Read More ►
As the automotive industry moves toward more automated, connected
vehicles, engineers are challenged to identify technologies that
can process and transfer large volumes of data in real-time...
Posted On 01/06/2021
Read More ►
The popularity of electric and zero-emissions vehicles is growing
substantially, although their share of the overall automobile
market remains relatively small. Automobile manufacturers are
spending...
Posted On 01/06/2021
Read More ►
Fluids play a critical role in sustaining life. Keeping animals and
humans hydrated and helping plants grow are obvious ways. Less
obvious ways include moving cargo around the world and...
Posted On 12/16/2020
Read More ►
Honeycomb air vent panels are used to help cool electronics with
airflow and while maintaining electromagnetic interference (EM)
shielding. Recently, our team of experts held a webinar on...
Posted On 12/03/2020
Read More ►
The growing connected vehicle and electric car markets are
currently driving up demand for IP-rated (Ingress Protection
rating) and EMI protection. Even standard road vehicle electronics
need to be...
Posted On 11/11/2020
Read More ►
What can be done if a bore requires radial sealing but lack of a
lead-in chamfer prevents the installation of a seal? A situation
like this occurs for instance when an existing bore should be
closed...
Posted On 10/22/2020
Read More ►
The advent of new and advanced technology has revolutionized the
space industry, ushering in a new era of innovation and change
brought by private space companies. Parker Chomerics was
recently...
Posted On 09/22/2020
Read More ►
As well as pharmaceutical production based on complex organic
molecules, manufacturing of advanced biologic drugs and vaccines
must ensure that in-process contamination risks are mitigated...
Posted On 09/21/2020
Read More ►
This is the second part in a two-part blog post series answering
the questions you asked during the webinar Selecting a Thermal Gel
or Thermal Gap Pad now, available on-demand. Missed part 1?
View it...
Posted On 08/27/2020
Read More ►
This is the first part in a two-part blog post series answering the
questions you asked during the webinar Selecting a Thermal Gel or
Thermal Gap Pad now, available on-demand. The objective of
thermal...
Posted On 08/20/2020
Read More ►
Clipper® Oil Seals are one of the Parker Engineered Polymer Systems
(EPS) Division's most widely used rotary seal products. They are an
effective solution – especially when used as direct...
Posted On 07/22/2020
Read More ►
The demand for dispensing thermal interface material (TIM) has
increased exponentially because dispensables offer engineers
flexibility in the designs and patterns that can be applied to
electronics...
Posted On 07/15/2020
Read More ►
Heavy duty equipment moves industry forward in all climates, from
the sunny Caribbean to icy Greenland. Effective, reliable sealing
is what allows hydraulic systems in heavy duty equipment to do
work,...
Posted On 06/25/2020
Read More ►
There are 400+ standard O-ring sizes, so which is the right one for
an application? Or maybe you are wondering if one O-ring
thickness is better than another. This question is posed to us
several...
Posted On 05/20/2020
Read More ►
In the rush to massively increase the number of ventilators
available to treat patients with severe cases of Covid-19, using
the correct seal materials for those ventilators should never take
a back...
Posted On 04/30/2020
Read More ►
Over the years, we've taken many questions from customers just like
you about the measurement and testing of our thermal interface
materials. How are they used? How are measurements determined?
What's...
Posted On 04/22/2020
Read More ►