Sealing Shielding

Sealing Fundamentals | Face Seal

Face Seal | Sealing Fundamentals - Parker TechSeal, Parker Hannifin, ApplicationsThe physics of creating a face seal is relatively simple. In most sealing systems, the objective is to prevent fluid from leaking from a high-pressure location to a lower pressure location through a sealing gap. Sealing fundamentals should be followed for trouble free application.

Creating a face seal

Static seals are typically subject to a preload to help attain sealability. Preload occurs when the seal height is designed to be greater than the sealing gap. Under compression, the seal is elastically deformed, producing internal stresses and generating a reaction force on both the top and the bottom of the sealing gap. When fluid pressure is applied, it causes additional internal stress, which supplements the preload and consequently prevents leakage.

An example of this phenomenon is illustrated in Figure 1 below by a Finite Element Analysis (FEA) simulation performed on an o-ring.

Face Seal - Sealing Fundamentals - finite element analysis FEA simulation performed on an o-ring

 

Figure 1 - Finite Element Analysis (FEA) simulation performed on an O-ring

 

In order for a face seal to function, the contact pressure between the gasket and the sealing interfaces at some location on both sides of the sealing gap and must be greater than the fluid pressure being sealed. In designing a face seal for a static application, there are three important factors to consider in addition to material selection:

Axial squeeze / preload:

The most critical design parameter is the axial squeeze, or the preload of the seal. The percentage of axial squeeze is calculated using the formula below:

 

Percentage of axial squeeze formula, compressed seal height, original seal height

Below is an example of FEA simulations for a rectangular cross section. Figure 2a on the left illustrates the uncompressed seal profile in the groove; Figure 2b on the right shows the seal characteristic when compressed in the groove. These simulations show that the seal height needs to be higher than the groove wall in order to achieve desired sealability. They confirm the importance of axial squeeze (or preload) in sealing.

Face Seal - Sealing fundamentals - Seal uncompressed in groove - FEA Parker TechSealSeal compressed in a groove - Parker Hannifin FEA

 

 

 

 

 

 

 

 

 

Figure 2a - Uncompressed seal profile in groove                     Figure 2b - Seal compressed in groove

Typically, the seal's axial thickness should be made such that it is deflected 25% of its original height when two mating surfaces that form the sealing gap are in their final positions at nominal conditions. It is important to consider the manufacturing tolerances of both the seal and the seal gap when designing. The suggested range of axial squeeze considering tolerances is 10 to 40%.

Gland fill

Gland fill is another important parameter to consider. Gland fill percentage is defined as the percentage of volume of the seal groove that the seal occupies. This percentage is represented by the following formula:

Gland fill % formula, Seal volume, Gland volume - Face Seal - Sealing Fundamentals

It is imperative not to overfill the gland. An excessive seal volume in a groove could cause damage to the seal and / or the sealing surfaces. The maximum gland fill recommended considering manufacturing tolerances is 95%.

Interference fit

The last characteristic that allows for the complete geometrical definition of a seal is the desired fit. Typically, if the higher pressure is located on the inside of the seal, an outside diameter (O.D.) interference with the gland is recommended. Conversely, if the higher pressure is located on the outside of the seal, an inside diameter (I.D.) interference with the gland is recommended. The interference should be designed in the range of 1 to 5% considering manufacturing tolerances.

It should be noted that sometimes it is not practical to design in an interference fit because of automated assembly or some other special consideration. In these cases, it is recommended to design in as little clearance as possible.

Subscribe to this Parker's Sealing and Shielding Blog RSS for more sealing fundamentals. Parker's Application Engineers can assist you with the material selection as well as the design process to ensure the optimal sealing solution for your applications. Please refer to ParFab Design Guide and O-ring Handbook for more information.

Consider reading some of these articles on sealing fundamentals, applications and trouble shooting tips:


Selecting the Right O-Ring Seal Squeeze Ratio

O-Ring Squeeze - More is Not Always Better

Sealing Fundamentals | How to Properly Install a Parker Hollow O-ring

 

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Sealing Fundamentals | Face Seal


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha