Sealing Shielding

Sealing Fundamentals | How to Properly Install a Parker Hollow O-ring

sealing fundamentals how to properly install a parker hollow o-ring, hollow o-ring, o-ring, low closure force, static seal, installing o-ring, o-ring installationAlthough appearing simple, the installation process of a hollow O-ring requires a proper method so that the seal fits correctly in the groove. This video provides instructions on how to properly install and uninstall a Parker TechSeal hollow O-ring. Following the installation instructions demonstrated in this video can help prevent overstretching the seal and therefore ensure the seal’s functionality.

Prior to the O-ring installation process, make sure the gland and the mating surfaces are clean and free of external contamination such as dust, debris, and other particles. The presence of those contaminants will create leak paths even when the seal is installed properly.

After the surface preparation step is completed, installing a hollow O-ring is fast and easy with two simple steps:

Step 1. Start at one point and work your way around the groove, pushing the seal into the groove.

Step 2. Once the seal is installed, lightly slide your finger around the seal to make sure that the seal is aligned correctly and evenly distributed along the groove track.

Seal replacement is also fast and simple: gently pull the old seal out of the groove and install a new one.

The incorrect method to install a hollow O-ring is to push the seal into the groove at one point and stretch the seal around the groove track. Stretching the seal will result in a fitting issue, inadequate sealing and ultimately seal failure.

For applications that need bolts or clamps to assemble the two mating components together, remember to use a star pattern to make sure that the compression force is applied equally on all points of the seal.

Parker hollow O-rings can be designed and manufactured in both standard and friction-fit series. Friction-fit means that the seal cross-section is oversized from the groove width, resulting in interference between the seal and the groove. The friction-fit feature enables the seal to remain inside the groove without the need for adhesives, O-ring lubricants or additional mechanical fasteners. This feature of Parker’s hollow O-rings is ideal for applications that would be inverted during assembly.

The friction-fit hollow O-rings are only compatible with grooves for friction-fit seals. Standard hollow O-rings, however, are compatible with most common O-ring grooves.

For more information about hollow O-rings, please visit the hollow O-ring website or call us at (864) 573-7332.

It's what you don't see that makes it a Parker O-ring. Be sure and bookmark our helpful, always-up-to-date online interactive O-Ring eHandbook.

 

Related Content:

Proper Installation of an O-Ring: Standard Male Gland

Proper Installation of an O-Ring: Standard Female Gland

Proper Installation of an O-Ring: Face Seal Gland

Proper Installation of an O-Ring: Full and Half Dovetails

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Sealing Fundamentals | How to Properly Install a Parker Hollow O-ring

ariiz
Nice blog thanks for share
thomasmoore
Hollow O Rings offer a low closure force alternative to solid O rings. The required elasticity is provided by the elastomer ring, the chemical resistance by the seamless sheath. Darcoid specializes in these hollow o rings.

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha