Sealing Shielding

Semiconductor FFKM Offers Low Particle Generation AND Extreme Etch Resistance

 FFKM Offers Low Particle Generation and Extreme Etch Resistance - silicon wafer - Parker O-Ring and Engineered Seals DivisionIn the world of semiconductor manufacturing, performance requirements are driving circuit sizes smaller and smaller, causing increased sensitivity to wafer defects. In parallel, the number of manufacturing steps has also increased driving a need for improved tool utilization and leaving more opportunity for these defects to be introduced. Identifying and eliminating the sources of defects is a tedious but necessary process to improve wafer yield.

 

What impact does seal contamination make?

One very distinct source of defects are the seals within a fab’s tool. Plasmas involved in both deposition, etch and cleaning processes utilize aggressive chemistries that put even high-functioning perfluorinated sealing compounds to the test. Much room for improvement has been left in this industry with many seal materials still posing significant threats to defectivity or downtime despite being designed for low particle generation or etch resistance.

 

How can Parker ULTRA change the industry?

Parker’s UltraTM FF302 Perfluorelastomer has proven success in CVD and etch applications, putting this material at the top of its class.  Typically, seal materials for semiconductor applications are optimized for low particulation or extreme etch resistance, however, Ultra FF302 provides both attributes in one material.  Laboratory testing shows Ultra FF302 has lower erosion in aggressive plasma chemistries even when compared to today’s leading elastomeric materials (Figure 1 below shows comparison erosion levels of various etch resistant perfluoroelastmers after exposure to Oplasma).

 

FFKM Offers Low Particle Generation and Extreme Etch Resistance - FF302 Perfluoroelastomer Erosion Comparison Chart - Parker Hannifin

Figure 1 

 

Not only has Parker’s Ultra FF302 shown promising results in the laboratory, but it has also had major success within the fab. In one field use, a fabricator was experiencing notable etching of industry-leading seals during a High Density Plasma Chemical Vapor Deposition (HDP-CVD) process involving SiH4 deposition with NF3 and O2 plasma cleans. Use of competitive materials (Competitor I, Figure 2) resulted in severe degradation with roughly 20% of the seal volume eroding; after the same period, FF302 O-rings experienced no erosion even in the most aggressive locations of the tool. (Figure 2 below shows the cross-sectional view of various FFKM O-rings after a full PM (60k wafers) on an HDP-CVD process).

 

FFKM Offers Low Particule Generation and Extreme Etch Resistance - FF302 Erosion Samples - Parker Hannifin

Figure 2 

 

If you are an equipment owner, you know this type of erosion is not unique to this fab alone.  As a matter of fact, Parker has seen this type of erosion across various fabs and various companies.

Resistance to any variety of etching of the sealing material is imperative. Physical and chemical etch often wears away the polymeric components of the elastomer, leaving behind organic or mineral fillers in a rough, abraded manner and dislodging larger particles. The successes of FF302-75 show its ability to resist the most aggressive etching and cleaning chemistries. For this very reason, more and more tool owners see Parker’s Ultra FF302 as a great solution for reducing the cost of ownership on the tools for which they are responsible.

For more information, visit Parker O-Ring & Engineered Seals Division online and chat with our experienced applications engineers.

 

 

FFKM Offers Low Particle Generation and Extreme Etch Resisance - Nathanael Reis, Parker Hannifin

This article was contributed by Nathanael Reis, applications engineer, Parker O-Ring & Engineered Seals Division

 

 

 

 

Other related content:

Perfluoroelastomer Materials Tailored for Your Needs

New CPI FFKM Extends Seal Life, Solving Long Time Industry Challenge

 

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Semiconductor FFKM Offers Low Particle Generation AND Extreme Etch Resistance


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha