Electromechanical

Series Hybrid Vehicle Electrical Systems

Previously, we discussed the advantages of the series hybrid vehicle architecture over parallel hybrid designs that results in superior fuel savings and reduced emissions. Now we will examine the electrical systems of the series hybrid.

The key to the series hybrid system is the conversion of the power generated by the electric motor coupled to the engine. The output from the motor (acting as a generator) is converted from a three phase alternating current (AC) at a variable frequency proportional to its running speed – to smooth direct current (DC) to charge the batteries and/or capacitor.  

The main traction drive motor, or motors, are typically induction or Permanent Magnet AC (PMAC) type. A bi-directional motor controller or inverter sources its power from the batteries and provides a variable frequency output to control the speed and torque of the main traction motor based on the driver’s command. 

Electrical System Components

The electrical system of most hybrid vehicles consists of the following subsystems: traction drive, Auxiliary Power Unit (APU), energy storage system, onboard diagnostics and vehicle control, and auxiliary equipment.Download this brochure.

  • Traction Drive Subsystem

This consists of the components that actually drive the wheels: electric motor or motors, bi-directional inverter(s), gear reduction system, driveline, and related components.

  • Auxiliary Power Unit (APU)  

The charging system consists of a gasoline or diesel powered Internal Combustion Engine (ICE), an electric generator, and related components.

  • Energy Storage System

This can consist of batteries, capacitors, fuel cells, or any storage or generating technology, along with the applicable monitoring, charging, equalization, and thermal control devices.

  • Onboard Diagnostics and Vehicle Control

These include battery management controls to ensure that charging is accomplished, dashboard displays, diagnostic tools, and related components. The accelerator and brake pedals interface with the power conversion components.

  • Auxiliary equipment  

In a typical series hybrid vehicle, this includes electrical power steering and braking systems, ventilation and air conditioning systems, and related components.

Continued improvements in battery design to enable higher power density, lower cost and better charge cycles, will be crucial to the continued progress of hybrid vehicle technology. For technical details, please reference this white paper: Basic Elements of the Series Hybrid Vehicle. 

 

Hybrid vehicle technology

The discussion on series hybrid vehicle technology spans three blog posts:

1. Series Hybrid Vehicle System Design

2. Series Hybrid Vehicle Electrical Systems

3. Advantageous Series Hybrid Technology Applications

 

Product and solution information is also available on the Parker Hybrid and Electric Vehicle website

This article has been provided by Lou Lambruschi, Marketing Services and E-Business Manager for Parker's SSD Drives Division and Energy Grid Tie Division.

Related Content:

Top Innovative Products and Systems for Heavy-Duty Vehicles  

Hydraulic Hybrid Fleet Approaches One Million Miles of Operation

 

Categories
Recent Posts by Author

Electromechanical and Drives Technology - A Look Back on 2019

Thanks to our loyal followers for all of the interest in the topics covered in this blog over the past year. In examining the most-read blog posts over the course of 2019, it becomes obvious that...

Time-Saving Solution for Servo Presses and Joining Applications

In industry, time is money. So, for engineers who are time-pressured, there is a solution for electromechanical press and joining applications. Push-To-Fit is an innovative electromechanical solution...

High-load Rodless Actuators Powering the Factory Automation Revolution

The arguments advocating more automation in our factories and process plants are gaining momentum and translating into a revolution in production environments.  Parker designs automated linear motion...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Series Hybrid Vehicle Electrical Systems


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha