Compressed Air Gas Treatment

Six Good Reasons to Dry Biogas to a Low Dewpoint Before Combustion in a CHP Engine

Six Good Reasons to Dry Biogas to a Low Dewpoint Before Combustion in a CHP Engine - Biogas processing facility - Parker HiRoss ZanderBiogas is renewable energy stored in organic materials, such as plant matter and animal waste, known as biomass. Sources of biomass fuel include agricultural residue, food waste, sewage, energy crops, landfills and animal waste. Anaerobic digestion is the process that occurs when bacteria decompose organic materials in the absence of oxygen for biogas power generation.

Biogas is primarily composed of methane and carbon dioxide with smaller amounts of other gases such as hydrogen, nitrogen or carbon monoxide which are often present in the gas mixture. Usually, the mixed gas is saturated with water vapor and may contain trace impurities such as hydrogen sulphide (H2S) and ammonia as well as dust or dirt particles. For biogas to be used as a fuel, most of these impurities must be removed as they may cause corrosion, deposits, and damage to equipment.

There are a number of benefits in drying biogas to a low dewpoint before combustion in a combined heat and power (CHP) engine.

The six major benefits of cooling to a low dewpoint include:

  • Increased CHP engine efficiency
  • Prevention of corrosion
  • Reduction of engine oil contamination
  • Increased service life of adsorbents
  • Partial removal of impurities such as H2S, ammonia, and siloxanes
  • Complies with technical instruction of all major gas engine suppliers

It is therefore essential to use a cooling system which has been specifically designed to produce low dewpoints and operate in aggressive ambient conditions such as those experienced in biogas applications. Read more about the benefits of cooling to a low dewpoint in this white paper.

Anaerobic digestion process

The anaerobic digestion process (see Fig. 1) as defined by the Anaerobic Digestion and Biogas Association is the simple, natural breakdown of organic matter into carbon dioxide, methane and water, by two groups of microorganisms, bacteria and archaea. Since many of these are intolerant to oxygen, this process is known as anaerobic. At the end of the process, we have a mixture of methane and carbon dioxide gases (biogas), water and some organic material (digestate).

Six Good Reasons to Dry Biogas to a Low Dewpoint Before Combustion in a CHP Engine - The Anaerobic digestion process - Parker Hiross Zander

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Fig. 1. Anaerobic Digestion Process supplied by Anaerobic Digestion and Biogas Association website

Biogas as an alternative fuel

The characteristics of biogas are comparable to natural gas. The energy content is defined by the concentration of methane. For biogas to be used as a fuel, most of the impurities have to be removed as they may cause corrosion, deposits, and damage to equipment. Impurities to be removed are water vapor, dust and dirt particles, and gaseous constituents. These gaseous constituents include hydrogen sulphide, CO2, halogen compounds (chlorides, fluorides), siloxanes and aromatic compounds.

It is generally accepted that a reduction in water content is beneficial to the CHP system, however traditional methods such as condensate traps and underground pipework cannot achieve low dewpoints which therefore reduces the benefit of removing water. For underground pipework to have any real cooling effect, long runs of pipe are necessary which is often impractical, expensive and difficult to maintain and service.

It is also common to use ‘air conditioning’ type chillers for biogas cooling but these units are not designed to produce low-temperature water and either result in higher gas dewpoints or end up operating well outside their design limits resulting in higher energy consumption and reduced service life. A cooling system should be used that is designed for biogas applications.

Speaker Presentation

Steven Scott presents at UK Anaerobic Digestion and Biogas ExhibitionDuring the 2013 UK Anaerobic Digestion and Biogas Exhibition, Steven Scott, market development manager - alternative energies for Parker's Hiross Zander Division / domnick hunter Filtration & Separation Division presented on selecting the right technology for CHP engines.  

Deciding which CHP technology to choose can be a difficult decision. A range of top technology providers discussed the issues such as

  • Cost, efficiency, and environmental impact;
  • Factors that may influence decisions;
  • What technology is available; and
  • Examples of how it is operating in practice.

Other experts presenting at the conference included:

  • Mark Moreton, NIFES Consulting Group
  • Ian Farr, Technical Sales Engineer, Edina UK
  • Ian Burgess, Sales and Project Management, SEVA Energie AG
  • Andy Cooper, Sales Engineer, Clarke Energy

For your review, here is Steven Scott's presentation from the exhibition.

 

 
Other posts related to compressed air and gas treatment
Categories
Recent Posts by Author

Is Your Compressed Air Purity Validated?

Is your manufacturing plant's compressed air purity validated? Perhaps the methods you are employing to check the purity or quality of the air in your facility are only indicative? Is there...

Six Points to Consider When Applying ISO8573-1 in a Manufacturing Facility

ISO (International Standards Organization) is the world’s largest developer and publisher of international standards. There are three ISO standards that relate to compressed air quality and testing...

Air Preparation for High-Precision Manufacturing

Today's global industrial, industrial and electronics manufacturing environment is uncompromising. To remain at the forefront, suppliers must meet a multitude of demands - shortest lead time, highest...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Six Good Reasons to Dry Biogas to a Low Dewpoint Before Combustion in a CHP Engine


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha