ISO (International Standards Organization) is the world’s largest developer and publisher of international standards. There are three ISO standards that relate to compressed air quality and testing — ISO8573 Series, ISO12500 Series, and ISO7183 Series. The most commonly used standard is the ISO8573 Series, in particular, ISO8573-1:2010.
ISO8573 is the group of international standards relating to the quality (or purity) of compressed air. There are nine parts to the standard. ISO8573-1 (part 1) is the most commonly used and relates to quality classifications for compressed air. Parts 2 - 9 specify methods of testing for a range of contaminants.
Here, we will discuss six essential factors to consider when using the ISO8573 Series Part 1 to maximize the effectiveness and efficiency of air treatment in your industrial manufacturing facility.
ISO8573-1 contains air purity classification tables that will provide you with guidance that specifies the minimum air purity required at each usage point, based on the types of contaminants you may seek to remove: solid particulate, water and total oil. See figure 1. From this table you can:
Figure 1 - Combined ISO8573-1 Table

In the ISO8573-1 table, compressed air contaminants are grouped as solid particulate, water and total oil. There are various degrees of each of these contaminants itemized to help in the selection of an appropriate combination of levels, based on your usage. These combinations are referred to as purity classes. When using ISO8573-1 to define the air purity required, it should be written in the following way:
Below is an example of an air purity specification:
ISO8573-1:2010 Class 1:2:1
Based on figure 1, this air purity specification would specify Class 1 particulate levels not to exceed 20,000 particles in the 0.1 to 0.5 micron size range, with additional levels at other particle sizes; Class 2 water levels identifying a pressure dewpoint (PDP) of -40 degrees Celsius, and Class 3 oil of no more than 0.01 mg of total oil.
In 2010, ISO8573-1 was updated with the inclusion of Class 0 to the three contaminants. See figure 2. Class 0 was introduced as a “customizable” specification that users and equipment manufacturers could use to identify a specific air quality that would be more stringent than Class 1. This has led to certain misrepresentations or myths. These include:
The following are the important facts to remember:
Figure 2. 2010 Classification Table (combined)

Of the three revisions — 1991, 2001, and 2010 — 2010 should be used when specifying a new system or upgrading a new system. However, if a previous revision has been used to specific purity levels, it is acceptable to continue using it, noting that changes in contamination levels require different purity equipment.
Parker, for example, offers a range of purification equipment that allows the user to specify the quality of compressed air for every application, from general-purpose ring main protection, through to critical clean dry air (CDA) point of use systems. Parker has comprehensive ranges of purification equipment available to exactly match system requirements, ensuring both capital and operational costs are kept to a minimum. Figure 3 provides an overview of Parker purification equipment required to meet or exceed the ISO8573-1:2010 classifications.
Figure 3. Overview of Parker purification equipment that meets or exceeds ISO8573-1:2010 classifications

Identify the quality of compressed air required for your system. Note that each point in the system may require a different quality, depending on the application. Refer your supplier to the quality classifications shown in ISO8573-1.
To maximize the return on investment in purification equipment, it is recommended that compressed air is treated for plant distribution in the compressor room to meet the broad needs of the facility. Point of use purification should also be employed with specific attention to the air quality required at each application. This approach assures the air is not over-treated and provides a cost-effective solution to high quality compressed air. Figure 4 shows an example of general purpose air with oil-free air for critical applications.
Figure 4. General Purpose Air with Oil-Free Air for Critical Applications

This article was contributed by Mark White, compressed air treatment applications manager, Parker Gas Separation and Filtration Division EMEA
Related content
Is Your Compressed Air Purity Validated?
How Oil Vapour in Ambient Air Affects Compressed Air Quality
Compressed Air Treatment Solutions for Today's Manufacturing Plants
Have a question about Parker products or services? We can help: Contact Us!
Comments for Six Points to Consider When Applying ISO8573-1 in a Manufacturing Facility
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.