Hydraulics

Solution for Capturing Maximum Solar Energy Includes Helical Actuator

Capturing Maximum Solar EnergyIn a Concentrating Solar Power (CSP) system, solar radiation is collected and concentrated, multiplying the sun's ambient heat to temperatures in excess of 750°F. In the most common application of CSP today, this is accomplished through parabolic troughs that use reflective mirrors to concentrate the sunlight onto receiver tubes that are connected in a vast plumbing system throughout an array of troughs. The receiver tubes carry a heat transfer fluid, which circulates along the length of each of the troughs and then into a heat exchanger, where the heat is extracted to make steam. The steam is used to create electricity using the same kind of generators that are traditionally driven by steam made from burning of fossil fuels. Currently, there are several parabolic trough concentrated solar power facilities operating in the Southwest region of the U.S.

Crucial to the effective operation of a parabolic trough is the ability to precisely position the concentrator for maximum solar energy capture as the sun moves across the sky. The focal point of the concentrated solar energy must be maintained directly on the receiver tube or the efficiency of the system drops off significantly. In order to maintain optimum efficiency, the trough must track the sun with precise controls and maintain accuracy to within 0.06° (1.0 mrad) with virtually no variation. This challenge becomes more difficult when dealing with the very large collector surfaces required. Each typical parabolic trough collector assembly has a total reflective area of 8,000 sq feet or more and must maintain tracking efficiency with wind gusts of up to 40 mph or sustained winds of up to 25 mph. The collectors also must operate in harsh conditions found in the deserts of the Southwest United States and across the world. Searing heat and dust are their constant companions. Component reliability and low maintenance requirements are a must.

 

Precise positioning

How To Capture Maximum Solar Energy Rotary Actuator Cutaway Cylinder DivisionOne solution was jointly developed by Parker's location in Enumclaw, Washington, and OnSun in Albuquerque, New Mexico. OnSun is an integrated tracking, control, and drive system for large solar power systems. OnSun is comprised of two major subsystems. First is a helical hydraulic rotary actuator with a sliding spline design. The unique design of its inherent helical gearing allows the rotary actuator to provide increased holding torque of up to 1.8 million inch-pounds, eliminating the requirement for an external holding brake mechanism found on alternative drive systems. The second subsystem is a sun-tracking control system, SkyTrakker, developed by OnSun. Delivered as a compact, pre-fabricated package, the integrated OnSun sun tracking system allows for rapid field installation and system start-up.

Solar energy collection is most efficient at the equator, where gross thermal solar power is approximately 1,000 W/m2 of direct solar radiation. Dependent on geographical location, 6 to 8 solar collector assemblies are required for each MW of electricity to be generated, and each collector assembly requires an individual tracking, control, and drive system. A modest 25 MW solar field will have as many as 200 collector assemblies, each with a drive system that consumes the very same electricity that is being generated. To minimize this energy consumption, the OnSun system uses a variable frequency drive control for the hydraulic pump motor that minimizes startup currents and reduces parasitic power consumption by 50%.

The heat transfer fluid is circulated through a mechanically coupled continuous loop system that traverses through multiple collector assemblies so synchronous coordination of the movement of each collector is vital. With state-of-the-art communications capability, SkyTrakker provides system health monitoring to ensure reliability and system life. High-speed remote monitoring and control are provided using field network communications between SkyTrakker and the control room. Both an RS- 485 optically isolated wired network and 2.4 GHz wireless RF network communications are provided. Heat Transfer Fluid temperature-monitoring capability is provided for high temperature and freeze mode protection. Both remote and local monitoring of the HTF is provided for dual safety operation. In addition, complete monitoring of each SkyTrakker operation is available using a USB connection for field maintenance and debugging operations.

As a better alternative to the complex and inefficient task of actually tracking the sun's position to maintain optimum collector efficiency, SkyTrakker controls the movement of the collector assembly by determining the desired collector position based on the sun's precisely known position in the sky relative to the exact location of the collectors on Earth. This ensures that the collector is always in the best position, even if cloud cover blocks the sun momentarily. As soon as the cloud or other obstruction clears, the collector is in precise alignment to resume maximum thermal efficiency and there is never a ’’hunt' mode due to the collector being off position. A solid-state digital inclinometer is used to ensure the tracking accuracy is maintained to within 0.05°.

The most precise and accurate positioning algorithms and controller would be of little value without a drive system capable of responding with accuracy to the minute positioning commands generated. The sun is in continual motion as it tracks across the sky each day and maximum solar efficiency is only attained when the collector is properly focused. The very large surfaces of the collector assembly require a substantial support structure. Even with state-of-the-art space frame type designs, these structures weigh in at several thousand pounds. Additionally, the large surface area of the collector acts as a sail in even a slight breeze.

Mentioned previously, the OnSun drive system uses a helical sliding spline hydraulic rotary actuator, specifically Parker’s Helac L30 series model 380. The L30 series and its legacy predecessors have been in volume production for 25 years with more than 100,000 units delivered to military, mining and heavy equipment customers for use in extreme operating environments. For this application the actuator design was customized and develops 380,000 inch-pounds of output torque at 3,000 psi and is capable of rotating the collector in precise 0.1° increments through the entire 240° of total rotation.

The L30 series helical rotary actuators use a low hydraulic displacement to drive through their rotation cycle, which facilitates the use of a small pump and motor to supply the high-pressure fluid to the actuator. The self-contained hydraulic fluid system is charged with multi-functional gear oil that ensures long gear life for both the pump and actuator. Strict fluid cleanliness standards are used during the production of the drive unit to ensure that the fluid used is of the highest possible cleanliness standards. As part of this process, each component is thoroughly cleaned prior to assembly and then the completed actuator is subjected to a computer-controlled cycle test where the fluid is analyzed for particulate size and quantity. The actuator is continuously cycled and flushed with fresh ultra-clean fluid until the cleanliness standard is achieved. This eliminates the need for filters, and an associated preventative maintenance headache, thereby contributing to overall reduced cost of operation for the entire solar collector field. Coupled with a small electric motor, with support for 110 Vac and 220 Vac single and three-phase power input, is a single gear pump that provides the hydraulic pressure needed to drive the actuator in both the low-speed tracking as well as high-speed stow modes.

The OnSun system is designed for rapid field installation based on the low number of parts that are involved as well as quick installation and assembly features incorporated into the design. The drive system is delivered as a compact, prefabricated package that allows for rapid field deployment.

 

Solutions for Capturing Maximum Solar Energy Includes Helical Actuator Jessica Howisey CYLSolution for Capturing Maximum Solar Energy Includes Helical Actuator Daniel Morgado CYLThis article was contributed by Jessica Howisey, marketing communications manager and Daniel Morgado, applications engineer, Helac Business Unit, Cylinder Division and was originally published by Solar Power World  

 

 

 

 

Related content:

New Hybrid Actuation System Ideal for Renewable Energy Applications

Hydraulic Power Units Control All Functions of Hydro-electric Turbine

Clean Hydraulic Fluids Are the Key to Top Performance

 

Have a question about Parker products or services? We can help: Contact Us!

Comments for Solution for Capturing Maximum Solar Energy Includes Helical Actuator


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha