Electromechanical

Specifying a Motor for a Hazardous Location? What You Need to Know

Specifying a Motor for a Hazardous Location? What You Need to Know | Grain Silos | Electromechanical & Drives Division, Parker Hannifin Hazardous locations are operating environments in which explosive or ignitable vapors or dust are present, or are likely to become present. It is normal for various processing applications where gas, liquid or dust will be present in enough volume to cause an opportunity for them to ignite and cause a fire and/or explosion. An example would be an automated paint spray booth where the vapors in the air would ignite from a spark, or from a motor’s surface temperature that was too hot. In such environments, special motors are needed to ensure that any internal fault in the motor will not ignite, or be a source of an ignition.

A risk assessment must be taken to classify potentially dangerous locations as hazardous environments. Equipment and materials must also be suited for use in these dangerous areas. Learning the commonly used terms and design criteria used to qualify equipment will simplify your specification process.

This is important to know and understand so that if your processes are defined as creating a hazardous environment, you can take the steps necessary to specify the correct equipment into your facility that will not create the potential for people to be injured or killed; or for damages to occur from using this equipment.

 

Specifying a MOtor for Hazardous Location? What You Need to Know - Download Whitepaper - Parker Hannifin

To keep this information on explosion proof motor classifications by hazardous locations handy, download our whitepaper.

 


What are explosion proof requirements for motors?

Specifying a Motor for a Hazardous Location? What You Need to Know | rotary brushless servo motor | Electromechanical & Drives Division, Parker HannifinExplosion proof requirements for servo motors are dictated in the United States by UL674 and in Europe under the acronym of ATEX. The following provides definition to the terms that are commonly used within each of the directives. Thereafter, information on the design criteria used to qualify equipment for use in these hazardous areas.

UL674

Under UL674 directive, hazardous locations are those areas where fire or explosion hazards may exist due to the presence of substances that are flammable, combustible, or ignitable. These locations break into classes and divisions and further defined by groups and temperature classifications.

 

Class definitions

Class I – created by the presence of flammable gases or vapors in the air, or flammable liquids, in sufficient quantities to be explosive or ignitable. Class I locations are further categorized by Division (Refer to chart 1) and fall into Group A through D. (Refer to chart 2).

 

Class II – created by the presence of combustible dust, suspended in the air, in sufficient quantities to be explosive or ignitable. Class II locations are further categorized by Division (Refer to chart 1) and fall into Group E through G. (Refer to chart 3).

 

Class III – areas, where there are easily ignitable fibers or flyings, are present. These include cotton lint, flax, and rayon as examples. The fibers in a Class III area are not likely to be in the air but can collect around machinery or on lighting fixtures. A Class III location can be categorized as Division 1 or 2.

 
These locations don't normally require hazardous-location motors. Specifying a hazardous-location motor for Class III locations is a common error.
 
Specifying a Motor for a Hazardous Location? What You Need to Know  | Chart 1 Divisions of Hazardous Conditions | Electromechanical Division, Parker Hannifin
 

Chart 2: Gas, vapor, and liquid groups

Relate to the Minimum Ignition Energy of the flammable substance and the location where it is installed. The lower the ignition energy required to ignite the gas, the more dangerous the environment.
 

Specifying a Motor for a Hazardous Location? What You Need to Know | Chart 2 Gas, vapor, liquid groups | Electromechanical & Drives Division, Parker Hannifin


Chart 3: Dust groups

Specifying a Motor for a Hazardous Location? What You Need to Know | Chart 3 Dust Groups | Electromechanical & Drives Division, Parker Hannifin

 

Temperature classification – “T-Codes”

The surface temperature or any part of the electrical equipment that may be exposed to the hazardous atmosphere should be tested so that it does not exceed 80% of the auto-ignition temperature of the specific gas, vapor or dust in the area where the equipment is intended to be used.

The temperature classification on the electrical equipment label will be one of the following (in degrees Celsius):

Specifying a Motor for a Hazardous Location? What You Need to Know | USA Degrees C Gas Chart | Electromechanical & Drives Division, Parker Hannifin


ATEX

ATEX consists of two European (EU) directives. They are:

 
• The ATEX 95 equipment directive 94/9/EC, equipment and protective systems intended for use in potentially explosive atmospheres;
 
• The ATEX 137 workplace directive 99/92/EC, minimum requirements for improving the safety and health protection of workers potentially at risk from explosive atmospheres.
 
 ATEX defines the hazards into subgroups which are defined as zones, equipment groups, gas groups, dust groups and temperature classes. The following is a definition of each:
 

Zones – Broken into gas and dust groups. Zones 0, 1, and 2 relate to gas, and zones 20, 21, and 22 relate to dust.

Zone 0 – a place in which explosive atmosphere consisting of a mixture with air of flammable substances in the form of gas, vapor, or mist is present continuously or for long periods, or frequently.
 
Zone 1 - a place in which explosive atmosphere consisting of a mixture with air of flammable substances in the form of gas, vapor, or mist is likely to occur in normal operation occasionally.
 
Zone 2 - a place in which explosive atmosphere consisting of a mixture with air of flammable substances in the form of gas, vapor, or mist is not likely to occur, but if it does occur, will persist for a short period only.
 
Zone 20 – a place in which an explosive atmosphere in the form of a cloud of combustible
dust is present continuously, or for long periods, or frequently.
 
Zone 21 - a place in which an explosive atmosphere in the form of a cloud of combustible
dust is likely to occur in normal operation occasionally.
 
Zone 22 - a place in which an explosive atmosphere in the form of a cloud of combustible dust is not likely to occur in normal operation, but if it does occur, will persist for a short period only.
 
 
Specifying Motors for an Explosion Proof Environment? Here’s What to Know | EX Series Explosion Proof Servo Motors | Electromechanical & Drives Division | Parker Hannifin
 
 

Equipment Groups – Broken into group I and II and further broken down by category. The category definition is based on equipment design for protection.

Group I – Intended for use in underground mines as well as those parts of surface installations of such mines that are endangered by fire and/or combustible dust.

•     Category M1 – ensures a very high level of protection.

•     Category M2 – ensures a high level of protection.

Group II – Intended for use in surface equipment that is, or can be exposed to hazardous conditions (fire or explosion).

•     Category 1 – ensures a very high level of protection against gas, vapor, mists, and dust that are present continuously, frequently, or for long periods.

•     Category 2 – ensures a high level of protection for use in areas in which explosive atmospheres caused by gas, vapor, mists, and dust are likely to occur.

•     Category 3 – ensures a normal level of protection for use in areas in which explosive atmospheres caused by gas, vapor, mists, and dust are unlikely to occur, or would happen infrequently.

 

Temperature Classes - relate to a flammable substance and its Auto Ignition Temperature.

Specifying Motors for an Explosion Proof Environment? Here’s What to Know | Temperature classes | Electromechanical & Drives Division, Parker Hannifin


Design characteristics for explosion proof equipment (UL674 and ATEX)

There are various design criteria that the manufacturer can incorporate into their design. What is chosen will dictate the hazardous environment that the equipment can be used in. There are 4 “General Principles” of protection against explosion. They include:

•      Explosion Containment - allows the explosion to occur but confines it to a defined area. A structure cannot fail from the explosion.

Specifying Motors for an Explosion Proof Environment? Here’s What to Know | Explosion Containment | Electromechanical & Drives Division, Parker Hannifin

•      Segregation - a method that attempts to separate or isolate the electrical parts from the explosive mixture. Practices include pressurization, encapsulation, oil immersion, and powder filling.

Specifying Motors for an Explosion Proof Environment? Here’s What to Know | Segregation method | Electromechanical Drives Division, Parker Hannifin

 

•      Prevention - a method that limits the energy, both electrical and thermal, to safe levels under both normal and fault conditions. Practices include Increased Safety, Intrinsic Safety, Non-Incendive (simplified) and Special Protection.

•      Increased Safety – must prevent the possibility of having excessive temperature or generations of arcs or sparks inside or outside the apparatus during normal operation. Accomplished by incorporating an elevated safety factor to all components that make up the apparatus (connections, wiring, the degree of protection of enclosure, etc.).

•      Intrinsic - the most representative of the prevention concept and is based on the limitation of the energy stored in an electrical circuit (the circuit is incapable of generating arcs, sparks or combustible thermal effects). Intended for process instrumentation applications where the power required is less than 30 volts and 100 mA.

•     Non-Incendive – similar to Intrinsic where the electrical apparatus is incapable of igniting a surrounding mixture during normal operation. They differ in that the non-incendive is not evaluated for safety under fault conditions, so as a result is not approved for Div. 1 environments. 

•     Special Protection - developed to allow certification of equipment that is not developed according to any of the existing protection methods. Can be considered safe for a specific hazardous location but must undergo appropriate tests and/or a detailed analysis of the design.

 

Safety first

Specifying a Motor for a Hazardous Location? What You Need to Know | Converting press | Electromechanical & Drives Division, Parker HannifinBy helping operations personnel and engineers better understand the many factors that go into hazardous duty motor selection, the risk of explosions in facilities can be substantially reduced. Understanding the commonly used terms and design criteria used to qualify equipment provides facility managers with assurance that their operations are safe and in compliance with applicable regulations.

If you're uncertain that your servo motor will be safe in the environment in which it must operate, always consult the motor manufacturer for assistance. Never guess when worker safety is at stake.

 

Specifying a Motor for a Hazardous Location? What You Need to Know | Download white paper | Electromechanical Drives | Parker HannifinTo keep this information on explosion proof motor classifications by hazardous locations handy, download our whitepaper.

 

Learn more about our options in explosion-proof servo motors by downloading our Explosion Proof Servo Motor catalog with complete product specifications.

 

Jeff Nazzaro, Gearhead and Motor Product Manager, Electromechanical Automation North AmericaArticle contributed by Jeff Nazzaro, gearhead and motor product manager, Electromechanical & Drives, North America.

 

 

 

 

 

Related, helpful content for you:

How to Achieve Safe Motion Control in ATEX Environments

Best Way to Dry Compressed Air in Hazardous Areas

Evolution of Fuel Tank Inerting for the Aerospace Industry

Simple Safety Steps to Follow When Installing a Nitrogen Generator

Categories
Recent Posts by Author

Electromechanical and Drives Technology - A Look Back on 2019

Thanks to our loyal followers for all of the interest in the topics covered in this blog over the past year. In examining the most-read blog posts over the course of 2019, it becomes obvious that...

Time-Saving Solution for Servo Presses and Joining Applications

In industry, time is money. So, for engineers who are time-pressured, there is a solution for electromechanical press and joining applications. Push-To-Fit is an innovative electromechanical solution...

High-load Rodless Actuators Powering the Factory Automation Revolution

The arguments advocating more automation in our factories and process plants are gaining momentum and translating into a revolution in production environments.  Parker designs automated linear motion...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Specifying a Motor for a Hazardous Location? What You Need to Know


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha