Fluid Gas Handling

Standard Testing for Hydraulic Hose and Fittings

Standard Testing for Hydraulic Hose and Fittings - Parker Hose Products DivisionThe process for testing and evaluating hydraulic hose is defined by SAE and ISO Standards, which contains various test procedures including change in corrosion resistance, hose construction integrity, burst, and impulse test.
 

Salt spray test

The salt spray (or salt fog) test is a standardized and popular corrosion test method for hydraulic fittings used to check corrosion resistance of materials and surface coatings. Salt spray testing is an accelerated corrosion test that produces a corrosive attack to coated samples in order to evaluate and compare the suitability of the coating for use as a protective finish.
 
Most commonly, the time taken for oxides to appear on the fitting samples under test is compared to expectations, to determine whether the test is passed or failed. For instance, the plating on Parker’s hydraulic hose fittings will meet or exceed 120 hours to white corrosion and 240 hours to red rust.
 
 
Stainless steel or advanced plating options are alternatives to avoid corrosion. Hose Products Division offers a variety of stainless steel fitting configurations as well as XTR coating, which provides more than seven times the SAE standard protection.
 

Burst test

A burst test is a hydrostatic pressure test of a hose assembly that determines the actual burst strength of the assembly. Any signs of leakage, bulging, coupling ejection or hose burst below the specified minimum rated burst pressure of the assembly are considered a failure.
 
Minimum burst values are used as one factor in the establishment of a reasonable and safe maximum work pressure. Maximum working pressure is one of the essential operating characteristics that a hose user must know and respect to ensure satisfactory service and optimum life.
 
The following are recommended guidelines regarding the maximum working pressure:
 
  • Water Hose up to 150 psi - 3:1 ratio
  • Hydraulic Hose for all other liquids, solid materials suspended in liquids or air, and water hose over 150 psi - 4:1 ratio
  • Hydraulic Hose for compressed air and other gases - 4:1 ratio
  • Hose for liquid media that immediately changes into gas under standard atmospheric conditions - 5:1 ratio
  • Steam Hose - 10:1 ratio
For additional safety precautions and abrasion resistance, it is recommended to utilize a hose sleeve or guard based on the application. 
 
 

Cold flex test

Hydraulic hose manufacturers rely on cold flexibility tests, using guidelines such as ISO 10619, to design and rate their hydraulic hose products. When tested, the sample’s hose or cover should not crack; and when warmed to ambient temperature, the test piece should not leak or crack when subjected to proof pressure.
 
Rubber blends in typical hydraulic hose are rated for cold weather operation to –40° F (–40° C). However, a number of hose manufacturers offer a wide range of products suitable for lower temperatures such as Parker’s low-temperature hydraulic hoses that are rated to –70° F (–57° C).
 
 

Impulse test

Impulse testing for hydraulic hose is one of the key predictions of hose life. Impulse testing involves the pressurizing or cycling of hose pressure, often times up to 133% of working pressure, at rates up to 1 cycle per second while the hose is held in either a 90° or 180° configuration. To pass the test, the hose must meet or exceed two times the minimum number of impulse cycles based on the applicable industry standard. Parker tests its GlobalCore 787 and 797 to twice the impulse (to 2,000,000 cycles). Although hoses are tested at higher than rated working pressures, it is for your safety and the life of the assembly to not exceed the published maximum working pressure of the hose and/or fitting.

A more severe version of this test involves holding one end of the hydraulic hose assembly while moving the other end of the assembly back and forth, most often referred to as the flex impulse test. Flexing applications are some of the most severe applications hose assemblies can face and a flexing impulse test is a very good indicator of assembly robustness. 

 

Kyri McDonough, Hose Products Division, Parker HannifinArticle contributed by Kyri McDonough, marketing services manager at Hose Products Division, Parker Hannifin.

 

 

 

 

Other related topics on hydraulic hose, hose application, and selection criteria:

The Love-Hate Relationship Between Hydraulic Hose and Chemical Compatibility
Decoding a Hydraulic Hose Layline
Five Most Important Factors You Need to Consider for Hydraulic Fittings
Hydraulic Hose 101: Fast Facts
Successful Hydraulic Hose Assembly Starts Here
Going to Extremes: A Closer Look at Hydraulic Hoses

 
Categories
Recent Posts by Author

What Is ISO 14001:2015 and Why Is It Important for Parker Precision Fluidics?

ISO 14001 is recognized as the international standard for environmental management systems and provides organizations/businesses with criteria to follow, which will identify, control, and reduce their...

New Miniature Proportional Valve for Next Generation Ventilators

  One of the most import medical devices created in the last century is the ventilator. The ventilator is critical for patients who cannot breathe on their own due to medical procedures or long-term...

How OEMs Can Improve Life Science Instrumentation Performance

Today, gas chromatography (GC), mass spectroscopy (MS) and similar life science instrumentation are contributing to results in drug discovery, drug development, forensic labs, and the next...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Standard Testing for Hydraulic Hose and Fittings

pitt
Salt spray corrosion test(Salt Spray Tester TU380) is a kind of test which mainly uses the artificial simulated salt fog environment created by the salt spray equipment to evaluate the corrosion resistance of products or metal materials.

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha