Fluid Gas Handling

State-of-the-Art Metallurgical Lab Helps Drive Product Safety and Reliability for Industrial Tube Fittings and Adapters

State of the art metallurgical lab helps drive product safety and reliability for industrial tube fittings and adapters

Corrosion. Rust. Metal fatigue. High-pressures. At Parker Tube Fittings Division, we recognize the harsh conditions where our products have to perform, so we established a state-of-the-art metallurgical lab where we test products in conditions that mimic our customers’ applications, using tools that include:

  • Ultra-high-pressure test stand capable of achieving up to 75,000 psi of pressure
  • Ingression tester to simulate pressure conditions that exist more than four miles below the ocean’s surface
  • Test chambers to evaluate the effects of water, salt and oxygen on component life
  • Equipment for tension and compression tests to measure the force required to pull apart fittings, up to an extraordinary 136,000-pound force 
  • Fatigue testing equipment which can cycle up to 200 times per second
     

Using magnification technology to understand how harsh environments affect material chemistry and coatings

More than just testing components for strength and durability under harsh conditions, we also use magnification to understand how those conditions affect the microstructure of materials and surface treatments such as coatings. Our magnification tools include an optical microscope for 3D image reconstruction (up to 2,500 times magnification) and a Scanning Electron Microscope (magnification up to 300,000 times), for resolving features down to 3nm and chemical composition down to 100 nm.
 

Meeting performance and safety standards and pioneering the development of robust, advanced products 

Using this equipment, we perform tests in accordance with SAE, ISO, ASTM, API and ASME, and have also performed tests under the guidance of DNV.

Our metallurgical lab also enables us to develop the most robust products possible, supporting the newest technologies in fluid power which demand higher pressures with no compromise on safety.

Watch our video, “State-of-the-Art Metallurgical Lab,” to learn more about how Parker’s Tube Fittings Division partners with our customers globally to safely pioneer fluid conveyance solutions that exceed testing standards and redefine what is possible.

 

Visit our Parker Tube Fittings Division website for product information, and follow our techConnect blog for posts from our engineering team on industry specific topics about hydraulic connections, fitting applications, technical tips and industry and standards related information.

Do you want to receive new product announcements and technology updates from Parker Tube Fittings Division? Subscribe today and stay informed

 

Related Content:

How Fittings with ToughShield Help Customers Save in Industrial Applications
What You Need to Know About Testing Your Hydraulic System for Particle Contamination
The Truth About Pressure Ratings for Hydraulic Fittings and Adapters

 

Categories
Recent Posts by Author

How Condition Monitoring Can Transform the Food and Beverage Industry

Our sense of taste is changing. We’re becoming more health conscious of the foods and beverages we consume to living a better life. No more perplexing and hard-to-pronounce food labels....

Frequently Asked Questions About Seal-Lok for CNG Fittings

Seal-Lok for CNG Fittings and Adapters provide reliable natural gas fuel conveyance in CNG applications with an O-ring face seal design that incorporates an elastomeric seal compound made of...

Any pressure. Any project. One solution. Infographic

GlobalCore is the future that OEMs and end users around the world have been asking for: a unified family of robust hydraulic hoses designed to endure the tough conditions where work gets...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for State-of-the-Art Metallurgical Lab Helps Drive Product Safety and Reliability for Industrial Tube Fittings and Adapters


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha