Fluid Gas Handling

The Advantages of No-Skive Versus Skive Hydraulic Hose Assemblies

Advantages of No-Skive Hose - Video - Parker Hose Products DivisionSkiving refers to removing (or shaving) part of the hydraulic hose cover and/or inner tube prior to attaching hose ends. No-skive means the hose and fittings are designed to work without this step. In other words, hose and fittings come ready to assemble. The big difference between skive and no-skive hose is in the thickness of the outer cover. The thicker cover requires a different hydraulic fitting shell due to the thickness. 


So what is the advantage to you?

With no-skive, the hose core is not exposed to possible damage since the cover or inner tubes do not need to be removed to attach the crimped fittings.  Also, a no-skive hydraulic hose speeds up the assembly time of a hose assembly, and there is no additional equipment or clean up needed. Furthermore, the correct combination of no-skive hose and fittings guarantees a total form lock connection between shell and reinforcement and assures a safe and leak-free long service life.

Advantages of No-Skive Hydraulic Hose -  fitting showing skive and no skive - Parker Hose Products DivisionNo-Skive hose also offers the following benefits:

  • Avoids premature hose failure caused by under or over skiving
  • Protects the steel wire reinforcement against corrosion
  • Offers an outer rubber cover to mechanically protect the steel wire reinforcement during hose fitting assembly
  • Includes engineered fittings where the teeth of the shell bite down to the wire provide a metal-to-metal grip
  • Eliminates costly skiving equipment

No-skive hose not only speeds assembly, it eliminates needing skiving equipment, wasted time and clean-up. No-skive hose assemblies are the preferred choice for all medium pressure mobile and industrial applications. Parker offers more no-skive hydraulic hose than any other manufacturer. 


Watch the short video clip below to see how no-skive hose can speed the hydraulic hose assembly process.

 

Kyri McDonough, Hose Products Division, Parker HannifinArticle contributed by Kyri McDonough, marketing services manager at Hose Products Division, Parker Hannifin.

 

 

 

 

Other related topics on hydraulic hose, hose application, and selection criteria:

Five Most Important Factors You Need to Consider for Hydraulic Fittings
Hydraulic Hose 101: Fast Facts
Top 8 Reasons Hydraulic Hoses Fail
Top 5 Reasons Customers Choose GlobalCore Hose
Successful Hydraulic Hose Assembly Starts Here
Going to Extremes: A Closer Look at Hydraulic Hoses

 
Categories
Recent Posts by Author

Install Transair Push to Connect Fittings In 7 Easy Steps

Push to connect fittings have grown in popularity due to their ability to efficiently couple fittings to thermoplastic tubing while maintaining performance. Invented in 1969, push-to-connect fittings...

Choosing a Solenoid Valve for Applications Requiring Extreme Performance

Today's state-of-the-art laboratory and medical instruments are smaller, more accurate and higher performing. Many applications, such as those in analytical chemistry (mass spectrometry and...

How Condition Monitoring Can Transform the Food and Beverage Industry

Our sense of taste is changing. We’re becoming more health conscious of the foods and beverages we consume to living a better life. No more perplexing and hard-to-pronounce food labels....
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for The Advantages of No-Skive Versus Skive Hydraulic Hose Assemblies


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha