Process Control

The Choice Between LNG and CNG as Transportation Fuel

The Choice Between LNG and CNG as Transportation Fuel - Parker Hannifin VerifloOf the many transport fuel choices available today, none plays a more strategic role than natural gas in having an immediate and major positive economic and environmental impact. But of the two most widely available – CNG and LNG – which is most appropriate?

Selection considerations

There are various considerations that affect fuel selection. Vehicle range, type of cargo, type of vehicle, driving conditions, turning radius, length and/or weight limitations all affect fuel choice. In the case of natural gas, the availability of infrastructure or supply chain and/or the cost of establishing these is key to the choice between LNG and CNG.

LNG applications – transportation and shipping

The market for LNG use in transportation and shipping is growing.

  • A large vessel carrying LNG may use LNG to propel it. Since evaporated cargo provides a source of clean fuel, most LNG tankers have a steam-turbine propulsion system, which can efficiently use the existing terminal infrastructure and the ‘boil over’ – the part of LNG that turns into gas due to heat absorption in tanks. The economic and environmental benefits will more than pay for the small loss of cargo.
  • For container ships, there are challenges to overcome for smooth transcontinental routes, but this is a significant area of potential for LNG.
  • In areas where LNG terminals are available, ferries have begun to use natural gas as a transport fuel. LNG is increasingly being used in response to new rules that require vessels in the Baltic Seal in Northern Europe and off the coast of North America to significantly reduce emissions of SO2 and other pollutants.
  • Offshore drill vessels are another good candidate for LNG, as well as for natural gas that would normally be flared off and burnt from a well.

LNG applications – inland

LNG is well-positioned for growth in inland applications as well. It is deployed to run rail engines, mining trucks, gas compression stations, and on-shore well equipment. Typically, a hub-and-spoke relationship drives growth, facilitating the adoption of the fuel by on-road long-distance trucks with access to LNG at their terminal points. According to NGV Global, which represents the natural gas vehicle industry, the success of LNG for heavy-duty vehicle and off-road applications, along with the advent of LNG-fueled marine transportation, will serve to push natural gas into new territory as it delivers significant economic and environmental benefit.

Cryogenic pump key to LNG use

Central to the fluid system design for LNG is a submersible cryogenic pump installed in the storage tank in fueling stations, as well as in some storage systems on vehicles or vessels. The pump moves LNG into the vaporizer, which gasifies the liquid. Aerospace pumping technologies, which have very low losses, are currently being tested for this application to limit heat loss and enhance the ability to use the whole tank.  Other systems use the pressure created in the tanks to move the gas out of storage. However, for larger engines with heavy demand or at fueling stations, a submerged cryogenic pump is preferable to move large volumes of gas.

CNG applications

The choice between LNG and CNG as transportation fuel - Truck image with Veriflo valve shown  - Parker Hannifin - Veriflo Division In recent years, CNG has grown in acceptance and use around the world due to strong endorsements from China and India, where it has been widely adopted as a public transport fuel. Spurred on by an increased availability of technology from Cummins Westport, Daimler, Volvo, Ford, and GM, as well as key systems providers, such as Parker Hannifin, AC Delco and Bosch, CNG has gathered strong momentum. 

  • In the U.S., fixed-route trucks such as beverage delivery vans, waste trucks, and cement mixers have increasingly adopted CNG as a fuel of choice, driven by larger-sized engines and long distances and performance demands.
  • As of 2013, there were over 120,000 natural gas reciprocating engines produced in North America, reflecting 10% year-over-year growth. In China, growth is running at 25% year-over-year.
  • CNG use and acceptance has been further advanced by the development of lighter weight, fully composite tanks, allowing on-road trucking to adopt CNG in a much bigger way

Conclusion

Markets are driving innovation in natural gas engines, storage, and fuel systems, with the aim of achieving near-zero emissions. Further innovations in fuel systems are focused on robust systems with improved stable flow performance, accurate flow and pressure control, and near-zero fugitive emissions to further reduce the carbon footprint of natural gas. Many forward-thinking organizations engaged in exploration and delivery are funding such efforts. The long-term goal is to reduce NOx levels of transport systems/engines to the same level as power plants (0.02 g/bhp-hr). This will potentially make natural gas vehicles and transportation cleaner than electric options.

Please review the areas that Parker has solutions for CNG and LNG and transportation applications.

Ask about our solutions for CNG and LNG applications.

Article contributed by Veriflo Division of Parker Hannifin 

 

Related resources:

Natural Gas Engines for Heavy-Duty Applications

New O-ring Face Seal Fitting Promotes Environmental Sustainability with Alternative Fuel Compatibility

Hydraulic Hybrid Technology Demonstrated on CNG Fueled Refuse Truck

Parker Veriflo CNG Dispensers Support Cleveland's Transition to CNG Buses

Clearing the Air on Global Emissions Standards for Non-Road and Marine Diesel Engines

Reducing Environmental Impact in the Waste Industry


 

Categories
Recent Posts by Author

Four Key Factors to Consider When Selecting Instrumentation Tubing

When designing a leak-free instrumentation system, one of the first steps to ensuring safety and reliability is to select the right tubing for the intended application. No system integrity is complete...

A Dangerous Mix - How to Avoid and Handle Mixed-Pressure Connections

Mixing high- and medium-pressure fittings or incompatible parts makes systems unstable, inefficient and potentially dangerous. At worst, it can cause a potentially fatal explosion. At Parker,...

It's Time to Recognise Integral Ended Connections on Instrument Manifolds

Securing leak-free connection of impulse lines to manifolds for applications that use differential pressure flowmeters is a subject that has taxed instrumentation engineers for more than a...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for The Choice Between LNG and CNG as Transportation Fuel


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha