Filtration

The Importance of Using an Air Receiver Tank in a Compressed Air System

The Importance of Using an Air Receiver Tank in a Compressed Air System - Compressor and Receiver Tank - Parker Gas Separation and Filtration DivisionAn air receiver tank is an integral and important part of any compressed air system. Typically a receiver tank is sized at 2 gal/scfm and increased to 4-10 gal/scfm of flow if there are big demand swings or surges. So, if a compressor has a rating of 25 scfm at 100 psig, the receiver tank should be 50 gals minimum up to 250 gals if there are large surges.

In a compressed air system, a receiver tank provides the following benefits:

  1. The receiver tank acts as a reservoir of compressed air for peak demands.
  2. The receiver tank will help remove water from the system by allowing the air a chance to cool.
  3. The receiver tank minimizes pulsation in the system caused by a reciprocating compressor or a cyclic process downstream.

Much like a water reservoir provides water during times of drought and stores water during the wet times, an air receiver tank compensates for peak demand and helps balance the supply of the compressor with the demand of the system.

Receiver tanks are required by law to have a pressure relief valve and a pressure gauge. The relief valve should be set to 10% higher than the working pressure of the system.

It is also important to install either a manual or automatic drain on the receiver tank to remove water from the system. A coalescing filter and air dryer are best placed downstream of the receiver tank. Read more about drying compressed air.

 

This post was written by David Connaughton, product marketing manager, Industrial Gas Filtration and Generation Division, Parker Hannifin.

 

Other related posts on compressed air and gas treatment:

Are You Ready for an Audit? Is Your Plant Compressed Air in Compliance with GFSI, SQF, and BRC Codes? Part 1 of 6

What are the Risks of Contaminated Compressed Air in a Food Plant? Part 2 of 6

How to Manage the Risks of Food Product Contamination from Compressed Air. Part 3 of 6

Is Your Food Product Safe from Microbial Contamination? Part 4 of 6

Understanding Good Manufacturing Practices for Compressed Air in Food Plants. Part 5 of 6.

What’s the Best Line of Defense against Microbial Contamination of Food? Part 6 of 6

Is the Compressed Air in Your Food Plant Safe?

Can Pressure Reduction Be Used to Dry Compressed Air?

Technologies for Drying Compressed Air: Aftercoolers and Coalescing Filters

How Manufacturers Find Savings in Compressed Air

Have a question about Parker products or services? We can help: Contact Us!

Comments for The Importance of Using an Air Receiver Tank in a Compressed Air System

syofyan
Currently we need the tank air receiver with specification as follow :

capacity = 500 l
pressure = 10 bar
c/w safety valve+manometer+ auto drain

Price fob singapore

we waiting your response soonest
Judy from the Gas Generation Team
Thanks for your inquiry. We will respond to your request for additional information via email. If you would like to speak with one of our application specialists, please call 800-343-4048 (US and Canada) or 978 858-0505
Jeffrey Mach
Your recommendation is a little confusing:
"Typically a receiver tank is sized at 6-10 times the flow rate of the system."

The units: volume vs. flow rate don't agree, so there is some critical unit information missing with your sizing factor.

The next sentence muddies the issue further with the compressor rated at 25 standard (not actual) cubic feet per minute at 100 psi (~6.8x compression means ~3.67 acfm). The receiver is sized at 150 cubic feet, but is that volume or air storage in scf (actually ~22 ft^3 volume)? In other words, if you were to store air at 200 psi, would the receiver be half the size?

It seems that you would want to size the receiver to store a quantity air, depending on how much you would use on typical demand, as you would with a hydraulic accumulator.

Can you help me understand your recommendation?
Relief Valve Release Annunciation
Nice! In a compressed air system, the use of air receiver is really important. As, compressed air can cause many harmful effects and hazards in the tank and surrounding. Thanks for updating people about this.After reading this post, they will be able to understand the need of air receiver.

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha