Bioprocess Pharmaceutical Filtration

The Role of Prefiltration in the Optimization of Bioprocess Filtration Systems

PrefilterFiltration is commonly used in biopharmaceutical manufacturing in order to control bioburden within the production process, and the appropriate use of prefilters can help to optimize filtration costs.

 

By employing a correctly selected and sized prefilter and positioning this upstream of a sterilizing-grade or bioburden control filter, the required area of these membrane filters can be significantly reduced.

 

The advantage of this? The cost of operating a prefilter and sterile filter with a low membrane area is generally less than the cost of operating high membrane area sterile filters without an upstream filter.

 

Key filtration requirements include:

  • High throughput
  • High capacity
  • Minimum system size
  • Minimum cost

 

Prefiltration media and applications

Prefilters suitable for use in biopharmaceutical applications can contain different types of filtration media – the appropriate media for use will depend on the application, as shown in the table below.

Selection table

 

 

 

 

Sizing prefilters

Sizing prefilters is technically difficult and time consuming – it can therefore be more effective for sizing to be performed on behalf of customers by filtration suppliers’ technical support groups.

 

Recommendations on the sizing of filtration systems that require prefilters:

  • Establish the requirement for prefiltration by sizing the downstream membrane filter.
  • Collate all existing relevant data on the properties of the process stream and perform experiments to determine the concentration and particle size of particulates and the viscosity of the process solution.
  • Select likely prefilter media based on the process stream and whether retention, compatibility or capacity will be an issue.
  • Select prefilter grades you expect to be most effective at protecting the membrane filter. For instance, a 0.2 micron filter is likely to require a prefilter with a micron rating of 0.5-0.6 microns, while a high capacity membrane filter with an integral prefiltration layer may benefit from a prefilter with a 

 

 

Parker Bioscience Filtration specializes in automating and controlling single-use processes. By integrating sensory and automation technology into a process, a manufacturer can control the fluid flow more effectively, ensuring the quality of the final product. Find out more at www.parker.com/bioscience

 

Related content

What is Sterilizing Filtration and Why is it Important?

How to Select the Right Filter for Your Bioprocess

Filtration and Biopharmaceutical Process Protection

 

Categories
Recent Posts by Author

Mycoplasma Contamination - Why So Serious?

Mycoplasma contamination poses a serious threat to biopharmaceutical manufacturers. But it's the specific characteristics of Mycoplasma that makeĀ it such a challenge. Mycoplasma characteristics differ...

Tackling the Source of Mycoplasma Contamination Biopharmaceutical Processes

Mycoplasma contamination can have a devastating effect on drug manufacturers but what are the factors make a bioprocess vulnerable to Mycoplasma contamination and what measures can be put in place to...

Listening, Learning and Applying Knowledge in Product Development

Although bulk filtration of a product prior to shipping was one of the first bioprocessing steps to benefit from single-use technology, it has been one of the last to benefit from...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for The Role of Prefiltration in the Optimization of Bioprocess Filtration Systems


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha