techConnect

The Truth About Pressure Ratings for Hydraulic Fittings and Adapters

The truth about pressure ratings for hydrualic fittings and adapters

Most people are aware that hydraulic fittings such as 37° Flare (JIC), O-Ring Face Seal, or Metric Flareless (DIN) tube fittings are designed to industry standards, such as SAE J514 or ISO 8434-1. These standards govern their dimensional characteristics. However, most of these standards also cover the performance requirements including pressure, temperature and corrosion resistance.  In the US, SAE standards governing hydraulic fittings, hose and tubing fall under the Fluid Conductors and Connectors Technical Committee and generally take precedence over International (ISO) or country-specific standards (DIN, BS).


Performance Standards for Hydraulic Fittings and Adapters

These standards have evolved over the years with many of the latest versions also specifying performance criteria to improve consistency in the market. For example, SAE J1453 Part 2, O-Ring Face Seal Fittings, states the following: “The connector assembly shall meet or exceed all applicable test pressures shown in Table 5 when tested at the torques shown in Table 6. Connectors shall pass the burst, cyclic endurance (impulse), vacuum and overtorque tests when tested per ISO 19879.” In addition to pressure performance requirements, SAE J1453 Part 1, shown in figure 1, provides guidance on working temperature (-40°C to 120°C) and corrosion resistance (96 h in accordance with ASTM B117). This standard makes it clear for fitting manufacturers and their customers what the fitting should be capable of, at least for carbon steel products.

SAE J1453 Standards Cover
Figure 1: SAE J1453 Cover

The requirements set forth in the standards, such as working pressure, are considered minimum design criteria and are often exceeded by some manufacturers, or modified for materials other than the standard carbon steel.  Aluminum is a popular material option; however, the standards do not directly cover performance requirements for aluminum. Therefore, by using the testing guidelines such as those in SAE J1453, a manufacturer can develop material-specific working pressure recommendations for fittings materials other than carbon steel that will meet the performance criteria.


The common approach to qualification of a new material typically has three steps:

Step 1 involves establishing the make-up torque for the new fitting material, which will be required for the next two steps. A good rule of thumb for this is to start with a multiplier of the ratio of the tensile strengths between the new material and low carbon steel. For example, aluminum has a tensile strength of about 30,000 psi, while low carbon steel tensile strength is about 60,000 psi. Therefore, a multiplier of 0.5 will be used to estimate the test torques in steps 2 and 3.

Step 2 involves a static pressure (burst) test per ISO 19879 to determine the failure pressure of the fitting using the make-up torques established in step 1. Using the minimum failure pressure of three test samples and dividing by four (4), a potential working pressure can be established with the required 4:1 design factor. An example of this is shown in table 1. Failure must be tube or hose burst (external to the fitting). If not, return to step 1 to evaluate the make-up torque and either increase or further decrease the torque depending of the failure mode.

Determining working pressure of hydraulic fittings from burst data
Table 1: Determining working pressure for hydraulic fittings and adapters from burst data.


Step 3 involves a cyclic endurance (impulse) test to one million cycles per ISO 19879. The pressure established in step 2 is multiplied by 133% and this value is used as the test pressure for the impulse test. In the table 2 example, the test was run at 5075psi x 133% = 6765psi. However, the final pressure was rounded down to 5000 psi for simplicity after the fitting test samples reached the end of the test without failure. If the fittings do not pass the test, either the pressure and/or torque will need to be adjusted, depending on the failure mode, and the test must be repeated. This step is repeated until all six test samples pass the one million cycle requirement. The final working pressure and make-up torque are based on the results of this test.

Determining final working pressure of hydraulic fittings from impulse data
Table 2: Determining final working pressure of hydraulic fittings and adapters from impulse data.


In addition to the burst and impulse tests, most fittings standards also require repeat assembly, leak, vacuum, vibration and corrosion resistance testing before a fitting can be fully qualified. The procedure described in steps 1-3 is required to ensure the other tests can be completed successfully.

How or whether a company tests all of the fittings it sells is important. The industry standard is testing for carbon steel fittings, but there are specific procedures and standards for stainless steel, brass and every type of material from which a manufacturer makes fittings. Additional testing does add to the cost of fittings, but these extra quality-assurance procedures help ensure product integrity. Any questions about product qualification or specific test results should be directed to your fitting supplier.

Do you have any tips or stories about pressure ratings to share? If so, comment below. If you have any additional questions or comments, please post them and I’ll respond if warranted. If you want to talk to me directly, I can be reached at Parker Tube Fittings Division, 614.279.7070 or via email.

Did you find this post helpful? Subscribe to TFD techConnect posts by email. TFD techConnect is a technically-focused monthly blog written for engineers specifically around motion and control engineering challenges.

Download a print-friendly version The Truth About Pressure Ratings for Hydraulic Fittings and Adapters.

Do you also want to receive new product announcements and technology updates from Parker Tube Fittings Division? Subscribe today and stay informed


Ted-Amling-Senior-Project-Engineer-Parker-Tube-Fittings-Division

 

Ted Amling, Senior Project Engineer, Parker Tube Fittings Division

 

 

 

Additional helpful content:

Sizing Tube to Maximize Hydraulic System Efficiency

Turn vs. Torque? How Making the Right Choice Keeps Your Hydraulic Fitting Connections Leak-Free

Four Easy Steps to Identify Hydraulic Threads

A Dollars and Sense Approach to Preventing Hydraulic Oil Leaks

 

 

 

Categories
Recent Posts by Author

Proper Assembly Steps for 37° Flare Fittings Using the Flats Method

Properly assembling your fitting connections help to ensure that your systems install and stay leak-free. This is why we have started a series of assembly posts/videos featuring the proper assembly of...

Proper Assembly Steps for Parallel Thread Adjustable Style Port End Fittings

Properly assembling your fitting connections help to ensure that your systems install and stay leak-free. This is why we have started a series of assembly posts/videos featuring the proper assembly of...

Assembly Instructions for Ensuring Leak-Free O-ring Face Seal Fittings

No matter what type of port, tube or hose ends your fittings have, it's important to know and use the proper assembly and installation steps. Today we are talking about O-ring Face Seal (ORFS)...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for The Truth About Pressure Ratings for Hydraulic Fittings and Adapters

kurt
Good writeup, but poor example of data/results. The data you provide indicates the hose is not capable of meeting the minimum burst requirement of 4xWP. Your data indicates you have a PpkU = -0.32 (you need a +1.33 to show that your PPM < 63).
Ted
Very good observation, and thank you for your comments. In practice such burst pressures would be further evaluated by either conducting additional burst tests with heavier wall tube to ensure a good statistical capability or the target working pressure would be reduced based on test results.
Cam
When you are rating a new coupling, are the burst tests performed on both halves of the coupling when uncoupled or just when the two halves are coupled together?
Ted
Thank you for your question Cam. Initial burst testing on our quick couplings is done in both the connected and disconnected states.

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha