Sealing Shielding

The Year in Review: Our Top 5 EMI Shielding Blog Posts of 2018

The Year in Review: Our Top 5 EMI Shielding Blog Posts of 2018, Top 5 EMI Shielding Blog PostsWe’re rounding up the most popular posts of the year on the Parker Chomerics EMI shielding blog in an effort to bid adieu to 2018 and give you our most useful, popular content in one spot.

Keep reading to see what made the cut!

5. Design Decisions Relating to EMC Shielding

When approaching the problem of electromagnetic compatibility (EMC), design engineers often consider it to be a secondary issue that can be dealt with once the device is working and, after all, it can be dealt with by putting a metal box around it! But that places mechanical engineers in a tough position as they deal with constraints such as weight, cost, performance and corrosion. Discover our best design tips to help with EMI shielding DURING the design stage! Read now.

4. Best Conductive Plastics: Five Things to Look For

Can electrically conductive plastics really replace traditional metal electronics enclosures? The answer is a resounding yes! There are very effective electrically conductive plastics available today that provide excellent electromechanical properties that help shield portable electronics from the electromagnetic interference (EMI) noise that is proliferating our daily life.

Smart phones, Bluetooth, Wi-Fi, radio, even your television are all susceptible to EMI. Discover the key points you may want to consider when evaluating electrically conductive plastics for your application. Read now.

3. The Difference Between Thermal Conductivity and Thermal Impedance

While not technically a blog about EMI shielding, thermal interface materials and EMI shielding generally go hand in hand. Thermal Interface Materials (TIMs) are useful for thermal management in electronic components, as they enhance heat transfer from a heat-generating component to a heat dissipater, or heat sink.

Across the industry, manufacturers often publish thermal conductivity in units of Watts / meter-Kelvin as well as thermal impedance in units of °C – inches2 / Watt on their datasheets. So, what is the difference between these two, and how should you consider them when selecting a TIM? Read on to find out!

2. Five Ways to Maximize Performance of Electric Vehicle Batteries 

Electric vehicles are developing fast in line with growing demand. However, only by selecting proven, reliable, high-quality products for the effective thermal management and EMI shielding of batteries, is it possible to maximize performance.

Discover how the EV market is changing the way we think about thermal dissipation and EMI shielding for automobiles now. Read more.

1. The Art of Spraying Electrically Conductive Paints

An oldie of a post – but clearly still a goodie! Electrically conductive coatings for plastic enclosure electromagnetic shielding are growing in popularity as concerns over weight increase for a variety of EMI applications in the military, aerospace, automotive, telecom, medical, and semiconductor marketplaces. However, conductive paints cannot be applied in the same way conventional paints are. Many first attempts do not go as well as planned. Learn more about how proper preparation and practice will make you successful in your application.

 

Parker Chomerics eNewsletter Sign Up

 

 

 

 

 

 

 

 

Jarrod Cohen

 

This blog was contributed by Jarrod Cohen, marketing communications manager, Parker Chomerics Division.

 

 

 

Related content:

Best Conductive Plastics: Five Things to Look For

Five Ways to Maximize Performance of Electric Vehicle Batteries 

The Art of Spraying Electrically Conductive Paints

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for The Year in Review: Our Top 5 EMI Shielding Blog Posts of 2018


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha