Over the years, we've taken many questions from customers just like you about the measurement and testing of our thermal interface materials. How are they used? How are measurements determined? What's the best way to characterize performance?
So we asked our engineers for help answering these questions. Read on to find out their answers.
Parker Chomerics’ standard test method of characterizing TIM performance is by ASTM D5470.
ASTM D5470 measures thermal impedance (resistance) of a flat disk-shaped specimen or controlled volume of a liquid TIM between two flat polished calorimeter surfaces under controlled load.
Apparent thermal conductivity is a calculated value that uses the thermal impedance (resistance) measured from ASTM D5470 and the sample thickness to calculate a thermal conductivity value. This value is influenced by how effectively the sample contacts (or “wets out”, if a dispensable) the calorimeter surfaces.
The thermal resistance at the interface between the sample and the probes is called contact resistance. Contact resistance adds to the overall thermal impedance (resistance) and may produce a lower measurement than bulk thermal conductivity.
Bulk thermal conductivity is an intrinsic property of any homogenous material. To measure bulk thermal conductivity, we must subtract the contact resistance from the individual ASTM D5470 thermal resistance measurements.
This is achieved by measuring thermal impedance (resistance) of the material at multiple thicknesses (at least three) and generating a straight-line plot. The y-intercept of that plot is the total contact resistance and the slope can be converted to bulk thermal conductivity.
A material can have a very high intrinsic bulk thermal conductivity but be outperformed by a material of lower bulk conductivity that is softer and conformable. Measuring apparent (effective) thermal conductivity can help better identify real world performance of a thermal interface material in many cases.
Generally, there is no “go-to” correction factor or simple equation to “convert” from apparent to bulk conductivity. The contact resistance can vary widely across different thermal interface materials and there are also many other factors to consider including pressure during test, flatness and thickness uniformity of sample, contact area, etc.
Both apparent and bulk conductivity are useful values for fully understanding a thermal interface material’s performance and expected behavior in application. It is useful to consider the bulk thermal conductivity as the maximum attainable thermal transfer efficiency parameter while apparent thermal conductivity values can offer an indication of how well the material performs in real world application where contact resistance cannot be ignored.
It is always difficult to compare values since it is unlikely that reported values from varying sources were generated using the same test method and parameters. There are many test instruments and methods used in the marketplace. Parker Chomerics relies on ASTM D5470 for accuracy and reliability.
The selector must be sure to consider test method used as well as any parameters used in the test that would influence outcomes (temperature, pressure, etc.). In addition, it is important to be aware of any “modified” methods reported. Without knowing the nature of the modifications, one can fall victim to overstatements of product performance.
Parker Chomerics reports bulk thermal conductivity for most TIM products on technical data sheets. Thin bond line products (such as phase change materials and thermal greases) data sheets will show thermal impedance at fixed pressure instead of bulk thermal conductivity as this is more practical and useful to the designer.
For lot-to-lot conformance testing, Parker Chomerics measures and retains apparent thermal conductivity and thermal impedance for every manufacturing lot of product.
This blog was contributed by Dana Drew, quality manager, Parker Chomerics Division.
Related content:
The Difference Between Thermal Conductivity and Thermal Impedance
Viscosity vs. Flow Rate - Which Is Best in Thermal Interface Materials?
Have a question about Parker products or services? We can help: Contact Us!
Comments for Thermal Conductivity Measurement Frequently Asked Questions (FAQs)
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.