Sealing Shielding

Thermal Pads: Which Layer Do I Peel Off?

Thermal Pads: Which Layer Do I Peel Off - Thermal Gap Pad - Parker ChomericsMost thermal pads, also known as thermally conductive gap filler pads, thermal gap pads, or thermal gap filler pads, have many different layer materials or carrier substrate options to choose from. It can be confusing which layer is supposed to stay on the product and which layer gets peeled off and removed before application. In fact, it’s one of our customer’s most asked about questions and can cause a lot of confusion on the manufacturing floor.

So, which layer should you peel off and which should stay on the thermal gap pad? Read on to find out.

Parker Chomerics, like many thermal gap pad vendors, offers several different gap pad layer options that must be peeled away before the gap pad is installed into the application. 

Think of a thermal gap pad as a sandwich of layers -- there is always a blue poly backing that keeps the gap pad together, but there are five additional carrier substrate options which provide the following benefits:


Thermal Pads Which Layer Do I Peel Off - Woven Glass - Parker ChomericsWoven fiberglass

The woven fiberglass carrier option provides reinforcement and a clean break / low tack interface surface, allowing for re-use of the thermal pad if necessary or for prototyping.

As you can see from the diagram, you peel off the liner to expose the woven glass carrier which does not get removed from the thermal gap pad.

Example: THERM-A-GAP HCS10G.

 

Thermal Pads Which Layer Do I Peel Off - Woven Fiberglass - Parker ChomericsAluminum foil with pressure sensitive adhesive (PSA) 

The aluminum foil with PSA carrier’s primary function is to allow a pressure sensitive adhesive on the thermal gap pad to affix the thermal pad in place.

As you can see from the diagram, you peel off the liner to expose the aluminum foil carrier which does not get removed from the thermal gap pad.

Example: THERM-A-GAP A579.

 

Thermal Pads Which Layer Do I Peel Off - PEN film - Parker ChomericsPolyethylenenapthalate (PEN) film 

The polyethylenenapthalate (PEN) film carrier permits the thermal gap pad to see a shearing motion and offers a clear, cost-effective dielectric film with fair thermal performance.

As you can see from the image at right, there is no clear film to peel off that exposes the PEN film carrier, which does not get removed from the gap pad.

Example: THERM-A-GAP 579PN.

 

Thermal Pads Which Layer Do I Peel Off - PEN film - Parker ChomericsThermally enhanced polyimide 

The thermally enhanced polyimide carrier permits the thermal gap pad to see a shearing motion and offers an excellent dielectric film with enhanced thermal performance. 

As you can see from the image at right, there is no clear film to peel off, the polyimide carrier does not get removed from the gap pad.

Example: THERM-A-GAP 579KT.

 

Thermal Pads Which Layer Do I Peel Off - No carrier - Parker ChomericsNo carrier   

The no carrier or “un-reinforced” option allows the thermal gap pad to have high tack surfaces on both sides, allowing for the pad to be highly conformable, but it does make cutting and handling of the product more difficult.

Once the liner is peeled back, there is no additional carrier on the thermal gap pad, the pad is now exposed.

Example: THERM-A-GAP 579.

 

Thermal Pads Which Layer Do I Peel OffBlue poly diamond carrier

Lastly, the base carrier liner, shown in blue, is persistent on the bottom of all thermal gap pad options, and must be peeled and removed prior to installation of the thermal gap pad.

This blue carrier is necessary, as it keeps the gap pad intact and more easily to handle prior to installation. We recommend keeping this blue poly carrier layer on just until the gap pad is placed for the final time.

 

 

 

Thermal Pads Which Layer Do I Peel Off - Thermal Interface Materials Catalog - Parker Chomerics

 

 

 

 

 

 

 

Thermal Pads Which Layer Do I Peel Off - Jarrod Cohen Author - Parker Chomerics

 

 

This blog was contributed by Jarrod Cohen, marketing communications manager, Parker Chomerics Division.

 

 

 

 

Related content:

How to Identify Quality Thermal Gap Fillers in Four Steps

The Four Best Thermal Interface Materials For Cooling Electronics

Viscosity vs. Flow Rate - Which Is Best in Thermal Interface Materials?

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Thermal Pads: Which Layer Do I Peel Off?


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha