Fluid Gas Handling

Top 8 Reasons Hydraulic Hoses Fail

Why Hoses Fail - Tube Erosion - Parker Hannifin, Hose Products DivisionThere are thousands of reasons a hydraulic hose can fail, but often, the most common failures could have been avoided with proper precautions. At Parker Hose Products Division, we work closely with customers regarding hose maintenance and failures, and we know how to protect your hoses, keep your machinery running and reduce costly downtime. Below are eight of the most common reasons for hose failure and how to protect against them.
 

1. Tube erosion

Hydraulic hose tube erosion often causes external leakage. Tube erosion is usually caused by a concentrated high-velocity stream of fluid or by small particles in the fluid. The red arrows in the image point to the start of the erosion.

In order to avoid tube erosion, use Hose Products Division’s flow capacity nomogram to determine the proper hose size based on the recommended maximum velocities. Also, be sure that the hose assembly is not bent too tight for flow and that the fluid medium is not too abrasive for the inner tube of the hose. It is important to follow the maximum bend radius noted in the engineering specifications for each hose, as well as diameter, during the assembly process.  
 

2. Fluid compatibility

Why Hoses Fail - Fluid Compatibility - Parker Hannifin, Hose Products DivisionSystem contamination and external leakage can be a direct result of fluid compatibility issues. Incompatible fluids will cause the inner tube of the hose assembly to deteriorate, swell, and delaminate. The inner tube can also partially wash out in some cases.  

The hose you order must be compatible with the fluid being conveyed. Verify that the fluid is not only compatible with the inner tube, but also the outer cover, fittings, and even O-rings. To ensure that your medium is compatible, check Parker’s chemical resistance chart for hydraulic hose. 
 

3. Dry air / aged air

Why Hoses Fail - Aged Air - Parker Hannifin, Hose Products Division

The inner tube of hoses can develop numerous tiny cracks due to aged or dry air. This type of failure is sometimes hard to spot because the hose will remain flexible, however there will be signs of external leakage. Typically, there are no signs of cracking on the hose under the fittings.

To avoid dry or aged air problems, confirm your hose is rated for extremely dry air. Hoses with inner tubes of PKR or EPDM rubber are preferred for these applications. If possible, raise the dew point of the air.
 

4. Minimum bend radius

Why Hoses Fail - Minimum Bend Radius - Parker Hannifin, Hose Products Division

Hose assemblies can fail relatively quickly if the minimum bend radius is not met. In this image, it is obvious that the tube and cover physically ripped apart at the outside of the bend, noted by the red arrow. The blue circle indicates where the tube and cover are buckled at the inside of the bend.  

In vacuum or suction applications, if the bend radius is exceeded, the hose may tend to be flat in the bend area. This will hinder or restrict flow. If the bend is severe enough, the hose may kink. To prevent minimum bend radius hose failures, double-check the recommended bend radius. Replace hose assemblies and change routing, length, or fittings to route the hose within the published minimum bend radius if they do not comply.
 

5. Insertion depth

Why Hoses Fail - Insertion Depth - Parker Hannifin, Hose Products Division

When a hose assembly is not properly assembled, it can create very dangerous situations. Fittings need to be pushed on completely to meet the recommended insertion depth. If the hose insertion depth is not met, fittings can blow off, leaving a failed hose assembly. The last grip in the fitting shell is essential to the holding strength.

To find the proper insertion depth, Parker offers easy-to-use hose insertion depth blocks to mark the hose. This will ensure that the hose is pushed on to the correct insertion specifications.
 

6. Improper assembly

Why Hoses Fail - Improper Assembly - Parker Hannifin, Hose Products Division

Contamination can cause several problems for a hydraulic hose assembly. When cutting a hose, metal particles and debris can settle inside the hose if not properly flushed. This abrasive debris left in the hose will contaminate the hydraulic system. It can also cause small fractures to develop on the inner tube of the hose assembly, resulting in leakage. 

To prevent hose failures from contamination, the hose must be properly cleaned before inserting the fittings. The inner tube should be “squeaky-clean” before fittings are inserted. After the fittings are crimped, be sure to cap the ends in order to keep the hose clean and avoid recontamination during transport. Parker offers hose cleaning kits and clean seal caps that provide a quick and easy way to reduce contamination, thereby reducing the risk of downtime resulting from clogged filters, component malfunctions and hose failures.


7. Heat aged

Why Hoses Fail - Heat Aged - Parker Hannifin, Hose Products Division

Hose failure can occur from overheating the hose assembly. Overheating will cause the hose to become very stiff. The inner tube will harden and begin to crack because the plasticizers in the elastomer will break down or harden under high temperatures. In some cases, the cover may show signs of being dried out. The hose assembly may remain in its installed shape after being removed from the application and if flexed, audible cracking can be heard.

In order to prevent overheated hydraulic hose assemblies, confirm hoses are rated for the temperatures required by your application. Also, reduce ambient temperatures or use heat guards and shields to protect the hose from nearby high-temperature areas.
 

8. Abrasion

Why Hoses Fail - Abrasion - Parker Hannifin, Hose Products Division

Hydraulic hoses are put through rigorous applications every day, which eventually take their toll. If not inspected on a regular basis, abrasion can cause a hose assembly to burst and leak. Excessive rubbing of the hose against an external object or even another hose can wear away the cover and eventually the reinforcement layers.

The cover is meant to protect the hose, so signs of damage to the cover or reinforcement layers should warn you that something is wrong. Protective sleeving is available to better protect against abrasion. Parker offers hose shields, sleeves, as well as protectors to meet the needs of a variety of applications. ToughCover and SuperTough cover options are also available, which eliminate the need for additional protective sleeving.

With a little background knowledge and training, many hose failures can be prevented. Ensure you are selecting the right hose to fit your specifications by using the STAMP (Size, Temperature, Application, Media, and Pressure) method. Parker’s Hosefinder app is the easiest way to narrow down precisely what hose you need with the STAMP process.

Properly assembled and installed hose assemblies will last longer, decreasing downtime and maintenance costs. If you need more information about extending the life of your hose assembly or if you need help determining the right hose assembly for your application, contact our customer service team by calling 440-943-5700, visiting parkerhose.com or find your local Parker distributor.

 

Kyri McDonough, Hose Products Division, Parker HannifinArticle contributed by Kyri McDonough, marketing services manager, and Derek Garceau, engineering manager at Hose Products Division, Parker Hannifin.

 

 

 

 

Derek-Garceau-Engineering-Manager-Parker-Hose-Products-Division

 

 

 

 

 

 

Other related topics on hydraulic hose, hose application, and selection criteria:

Top 5 Reasons Customers Choose GlobalCore Hose

Global Collaboration Delivers Unprecedented Hose Solution

What is an Onsite Container?

How to Choose the Right Fluid Power Hose

 

Have a question about Parker products or services? We can help: Contact Us!

Comments for Top 8 Reasons Hydraulic Hoses Fail

Zequek Estrada
The eighth cause for hydraulic failure really goes to show how important it can be to maintain proper maintenance. It's funny how things like abrasions can be prevented by simple means. Although, it's always good to know where you can get repairs even if you're keeping up with maintenance.
Michael Nyirenda
Wow. So helpful hose failure analysis information. Thanks send me a PDF copy on the same topic and any hydraulic failure analysis flow directions.
Wendy Soucie
Michael, you can easily print your own pdf of the blog post for your reference using the print feature at the top of the blog page. You will have a choice of print or pdf.

Regards, Wendy Soucie
CHEWE
this is helpful,please send me more notes.
otukei
May you kindly send copy in pdf about the same topic.Thanks
rich Yanzsa
Q: Can I use this in my hydraulics maintenance class giving credit to PH for this work? We stress proper hose install. and care all the time in our hyd. maint training class.
Kyri McDonough
Hi Rich,

That would be an amazing compliment if you did you use. Thank you for seeing the value in the blog.
Regards,
Kyri
A. Thomas.
operating in very hot dry atmosphere constant sun. will it help protect hoses from cracking to clean with old hydraulic fluid?

Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha