Sealing Shielding

Top Three Design Tips for Corrosion Resistant EMI Protection

Top Three Design Tips for Corrosion Resistant EMI Protection, Corrosion ComparisonEvery design engineer should know that an EMI gasket must be installed between mating flanges to prevent electromagnetic radiation (EMI) from entering or leaving an electronic enclosure. But what if your equipment will be used in humid or tempest environments? How confident are you in your design that corrosion protection will be addressed? Not so much? Well, then read on. Here’s our top three design tips for ensuring corrosion resistant EMI protection.

  1. Choose the correct EMI gasket. Sounds simple, right? But oftentimes, design engineers think they’re picking the right EMI gasket when in fact, they’re not. Correct gasket selection can minimize the difference in electrochemical potential relative to the structural metal, which in turn will slow down corrosion by ensuring a lower galvanic current. 
     
    You’ll want to select an elastomeric EMI gasket, such as the Chomerics CHO-SEAL® family, that contains conductive filler particles which will provide a combination of EMI shielding and corrosion resistance when in contact with metal. Pure silver, silver-plated copper, silver-plated aluminum and nickel-plated aluminum are among the particle types which have an important influence on corrosion resistance.
     
  2. Don't forget to choose a surface treatment. To maintain aesthetics and stop oxidation and corrosion, you’ll probably plate or paint your metal enclosure and finish flange surfaces to ensure protection against corrosion. But what you might not know is that you’ll want to select an additional coating system that prevents surfaces from corroding in those high humidity or marine environments.
     
    CHO-SHIELD® 2000-series coatings from Parker Chomerics are three-part, copper-filled urethane coating systems, which minimize the effects of galvanic corrosion due to the soluble chromates they contain. When paired with the fluorosilicone binders of CHO-SEAL® 1298, the combination delivers elevated resistance to galvanic corrosion. 
     
  3. Secondary sealing might be necessary. So you’ve got your elastomeric EMI gaskets and your corrosion resistant coatings, think you’re all set? Maybe not. Best design practice also indicates that an additional moisture seal should be considered if there is a requirement to exclude salt fog or spray that could act as an electrolyte and lead to corrosion.
     
    For example, in aircraft applications, a seal-to-seal design may be used. Here, gaskets of identical material are applied to each mating flange and edge-sealed using a non-conductive sealer to prevent moisture from entering.

Top Three Design Tips for Corrosion Resistant EMI Protection, Conductive Elastomer Engineering HandbookSo what have we learned? When you deploy a carefully selected combination of EMI gaskets, conductive coatings and secondary sealing, design engineers are able to minimize or limit corrosion to deliver sufficient EMI shielding performance for the service life of the equipment.

Are you ready to start choosing your EMI gasket? Download our Conductive Elastomer Engineering Handbook today and you'll learn: 

  • EMI shielding theory
  • Corrosion resistance principles
  • Conductive elastomer gasket design
  • Parker Chomerics elastomer product guides
  • Industry organizations and standards
  • Parker Chomerics capabilities and offerings

For more information on the Chomerics Conductive Elastomer Engineering Handbook and other Chomerics offerings, please visit our website or contact us

 

Top Three Design Tips for Corrosion Resistant EMI Protection, Tim Kearvell, Chomerics Division Europe

 

This blog was contributed by Tim Kearvell, elastomer product manager, Chomerics Division Europe.

 

 

 

 

Related content:

New Essential Handbook for EMI Shielding Applications

Interesting New Developments in Commercial Aerospace Gaskets

Improved EMI Shielding Consistency of Single Pellet Conductive Plastics  

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Top Three Design Tips for Corrosion Resistant EMI Protection


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha