Today, in the midst of the COVID-19 pandemic, keeping workers, patients and families safe from the spread of disease in facilities is more important than ever. For facilities managers, this means employing various strategies that can reduce the threat of transmission in:
- Industrial manufacturing plants
- Hospitals and healthcare facilities
- Commercial office buildings
- Hotels and entertainment complexes
- Food processing facilities
- Microelectronics manufacturing plants
- Data centers
- Schools and universities
- Clean manufacturing facilities
- Government institutions
Know how the disease spreads
The spread of the novel coronavirus (COVID-19) mainly occurs through respiratory droplet transfer from person-to-person within a close range of about six feet according to the Center for Disease Control (CDC). The virus can be transmitted on skin, objects, and surfaces that a contagious person may cough on, sneeze on, or touch.
Pathogens can also travel on dust and dirt particles as those particles move through the air. Therefore, the potential for airborne transmission through an HVAC system exists.
As part of a protection plan, maintaining healthier breathable air in facilities can help to reduce the risk of infection.
HVAC air filtration
To support a comprehensive protection plan that reduces the risk of airborne transmission for hospital staff and patients, TFS offers a range of high-efficiency filters that:
- Offer the highest level of protection - up to 99.999% on 0.12 microns.
- Provide 90% and higher efficiencies, capturing airborne particles that are the size of viruses.
- Meet LEED requirements and are designed for commercial use.
HVAC filters can reduce but not eliminate the threat of infection. The coronavirus and the particulate it travels on is very small in size and can range from sub-micron (less than 1.0 micron in size) and larger. High-efficiency filters on the market today can trap particulate sizes that are likely to remain in the air. Selecting the right filter can reduce risk while improving the quality of indoor air.
IMPORTANT: The filtration products TFS supplies can reduce airborne particulate in a controlled environment. They would not eliminate the risk of exposure to airborne viruses but can be part of a comprehensive plan to help reduce that risk.
Filtration guidance from the experts
The American Society of Heating, Refrigerating and Air-Conditioning Engineers (ASHRAE) has developed proactive guidance for building industry professionals to help address the ongoing concerns of the coronavirus (COVID-19) outbreak. Please visit www.ashrae.org to access the latest response resources from ASHRAE/Covid19 and other leading organizations with respect to the operation and maintenance of HVAC systems.
Recommended filters for reducing airborne risk
Our selection of HVAC filters from Parker are manufactured in the U.S. and engineered to the highest standards of design, quality, and assembly. When selecting a filter to combat the threat of airborne transmission, we suggest a minimum efficiency reporting value (MERV) rating of 13 to 16. The higher the value, the better the filter will be at capturing small particles. Our Sub-HEPA, HEPA, and ULPA filters provide the highest level of protection (up to 99.999% on 0.12 microns). Our MERV 16 rated filters provide 90% and higher efficiencies, capturing airborne particles that are the size of viruses.
The following high-efficiency filters are designed for commercial use. All of them meet Leadership in Energy Design (LEED) requirements. Request a quote by visiting our COVID-19 Reopening Support page.
Sub-HEPA, HEPA, and ULPA and pathogen barrier filters
Parker MICROGUARD® & MICROPLEAT™
- HEPA Filters: 99.97% and higher on 0.3 micron particulate
- ULPA Filters: 99.999 and higher on 0.12 micron particulate
- Best solution for hospitals, analytical labs, and clean rooms
Parker MICROGUARD® LR 12" Sub-HEPA Filters
- 98.5% efficiency on 0.3 micron particulate
- Proprietary E-Pleat® embossed media technology
High-efficiency filters
Parker Airguard® VARI+PLUS® (MERV 16 and MERV 14)
- 4-V mini-pleat filter
- Non-woven fiberglass media
Parker LoadTECH® Rigid Cell Filters (MERV 14)
- 4" and 12" sizes
- Proprietary E-Pleat® embossed media technology
Parker ADVANTAGE® 2" Mini-Pleat Filters (MERV 16 and MERV 14)
- Captures viruses, mold spores, and bacteria from 0.5 to 1 microns
- Best solution for hospitals, analytical labs, and clean rooms
Parker DP-Green Extended Surface Pleated Filters (MERV 13)
- 2" depth
- 100% synthetic media resists moisture
- Heavy-duty beverage board frame
Read more articles:
Is Air Bypass Costing You Money?
5 Factors to Consider When Selecting a Pleated Air Filter for an HVAC System
Comments for HVAC Air Filters Help Facility Managers Reduce Transmission of Infection