Quick and Easy Compressor Room Equipment Protection

Equipment Protection: Quick and Easy - Unprotected Air Intake - Total Filtration ServicesAssistance and recommendation from Total Filtration Services (TFS) to protect customer equipment in a compressor room using the Permatron Prevent System resulted in significant process improvements and cost savings for an automotive supplier based in Grand Rapids, MI. This blog will review the case study to learn how easy it is to protect your equipment by using the correct filtration products.

 

The challenge

The customer is a Tier-1 supplier to the automotive industry located in Grand Rapids, MI. They manufacture automotive interior, exterior and wheel trim and have several facilities with applications requiring filtration.

While visiting one of the customer’s facilities, they asked TFS to enter the compressor room to see if our team could supply the intake filters on their compressor units. Upon reviewing the application, TFS observed the current solution included the use of bulk rolled polyester media, which was manually cut by the maintenance team to fit each unit.

While able to supply the media, TFS informed the customer of the air bypass issue the current solution was producing, as the media wasn’t always cut accurately and often didn’t fit into the frames. As a result, each unit was at risk of being corroded and causing compressed air tools and equipment to fail.

Are you experiencing similar issues with your equipment? Connect with TFS here!

 

The TFS solution

TFS recommended the customer apply the Prevent System from Permatron, which is a vinyl screen sized to fit each unit and applied magnetically for easy installation and removal. The Prevent screen is a washable filter that can be re-used by simply blowing-off dust and debris with compressed air or washing with detergent if oils are present.

The TFS sales rep had samples of the Prevent screen and was able to show the customer how they could not only improve the level of protection for their equipment but also improve efficiency by eliminating the manual cutting process.

The customer followed the recommendations provided by TFS. Each unit was measured so screens could be supplied at the exact dimensions needed to prevent bypass. Upon receiving the product, the customer was impressed with how easy it was to install the Prevent, as Permatron's innovative system requires no drilling or tools. By using magnets, the Prevent System was easily installed and can be removed in minutes, without the need for special service or equipment shutdown.

For customers without metal, the Prevent System can be adhered by using a steel plate adapter with high strength tape adhesive that can be permanently affixed to the surface.

 

Equipment Protection: Quick and Easy - Prevent System supplied by TFS - Total Filtration Services

 

The results

Since being applied, the maintenance team is extremely satisfied with the new solution and plan to order a spare set of screens for each unit. They are also considering using the product throughout their facility to ensure all equipment is protected at all times.

TFS was able to recommend a solution that went beyond the customer’s initial request and lowered the total cost of ownership in the following ways:

  • Customer equipment and tools are adequately protected and are no longer at risk of being clogged with debris which required costly repairs.
  • Elimination of manual cutting of media allows the maintenance team to re-allocate resources and avoid potential injuries from repetitive motion and lacerations.
  • Eliminated waste resulting from both excess and dirty media.
  • Achieved cost savings by using a re-usable product instead of continually replacing media.

 

Watch this short video below to learn more about the Permatron Prevent System:

Click HERE to learn more about the Permatron Prevent System and how TFS can help you achieve cost savings. For more information about TFS and our product offerings, visit our Total Filtration Services website.

 

This blog was contributed by the Total Filtration Services Team.

 

Read more articles:

Resolving a Fouling Issue for a Wind Turbine Manufacturer

 Is Air Bypass Costing You Money?

Comments for Quick and Easy Compressor Room Equipment Protection


Leave a comment





Captcha