The company involved in this case study is a multi-national manufacturer of wind turbines that meets the needs of alternative energy production worldwide. Despite having the turbines installed in the ideal location, seasonal conditions brought upon a unique set of issues that required technical support to resolve. Continue reading to learn how TFS partnered with the customer to resolve their concerns with a simple but effective filtration solution.
The challenge
The customer had an installed a base of turbines in areas that are often flat and sparsely inhabited. As it turns out, these optimal conditions often occur in farmlands. In those areas where corn fields are nearby, seasonal conditions can lead to corn pollen entering the turbine compartment and fouling the impeller.
This fouling impacts the speed/efficiency of the turbine’s rotational energy leading which in turn, triggers an alarm on that particular unit.
Are you experiencing similar issues with your equipment? Connect with TFS here!
The TFS solution
The previous solution to this challenge required the owner of that unit to send a technician to the location to clean the unit. This entailed traveling to the often-remote location, climbing the tower to enter the unit, cleaning the foulant and then resetting the alarm. In several cases, during the peak pollination season, this was a daily occurrence.
TFS, working with one of its many trusted manufacturing partners, Permatron, proposed the installation of their PreVent screens at the inlets to their turbine’s impeller enclosures. The PreVent technology incorporates an electrostatically-charged material that enables the attraction/capture of airborne particles much smaller than the mesh size of the screen while having a negligible effect on air flow.
TFS worked with the customer to best identify those locations that might see the best use of these filters and helped to specify the correct size and model of PreVent screen.
The results
The most obvious benefit discovered by the customer after installation of the PreVent screens was the reduction of alarm events due to seasonal pollen issues. In fact, even those areas with daily alarms saw zero alarms after installation.
The customer experienced not only a reduction in the labor/time spent on addressing these daily occurrences, but increased energy conversion as the pollen no longer impacted the efficiency of the turbines/impellers. As the PreVent screens are washable/reusable, the customer now incorporates these filters on most new installations as a standard practice.
To learn more about how the PreVent system can help protect your equipment and achieve cost savings, submit a short form HERE.
This blog was contributed by the Total Filtration Services Team.
Read more articles:
Quick and Easy Compressor Room Equipment Protection
Comments for Resolving a Fouling Issue for a Wind Turbine Manufacturer