Parker United Kingdom

Improve Hydraulic System Profitability with a Free Temperature Test Kit

Improve Hydraulic System Profitability with a Free Temperature Test Kit | graphic for temp check - Parker HannifinThere are many underlying factors working in the background that, alone or in tandem reduce hydraulic system efficiency and drain overall profitability. To counteract, Parker is offering you a pre-assessment of your hydraulic system's efficiency, providing a free temperature test kit. This will help to identify where excessive heat could be costing you money for:

  • greater maintenance costs,

  • reduced productivity, and

  • increased energy bills.

Request a free temperature assessment kit today.

 

Watch the video and see the problems associated with excessive temperatures in a fluid tank and how to use the temperature test kit to identify if there are potential savings to be made on your hydraulic systems.

 

How can temperature control impact your profitability?

Under-estimation of heat dissipation – wrong assumptions of hydraulic cycles, neglected exothermic function of hydro-pneumatic accumulators, lamination or friction not properly calculated – lead to hydraulic fluid stabilizing at higher temperatures than expected. Despite progress made by oil industries to improve the performance of mineral oils and other fluids at elevated temperatures, the fluid lubrication capability will likely decrease.

Consequently, mechanical parts in motion will wear at an accelerated rate. This generates particles; impacting oil cleanliness and will start damaging servo valves and sensitive hydraulic components. The cycle continues: the more components get eroded the more abrasive the fluid becomes. The direct consequence is the impact on hydraulic component lifetime. Moreover, continuous operation at high temperature stimulates aging of rubber seals.

Eventually lower viscosity increases internal leakages, consequently, the system requires more power consumption for the same power output.

Owners risk facing unexpected leakages, reduced system efficiency, shorter interval between tank oil renewal or accumulators’ pre-charge controls, early product failures; those generating direct maintenance costs (human and material), loss of productivity and an increase of operational costs. Ultimately, a poor cooling design for a hydraulic installation impacts a customer’s business profitability.

Improve Hydraulic System Profitability with a Free Temperature Test Kit \ L-Series Air Oil Cooler | Accumulator and Cooler Division EuropeWith a wide selection of product ranges – air oil coolers, brazed plate heat exchangers and shell and tube heat exchangers – Accumulator & Cooler teams support their customers to size and select the most suitable product for their application. For more product information please visit our Cylinder and Accumulator Division Europe website.

You can get everything you need to keep cool from Parker.

 

  

This blog was contributed to by Erwan Jagueneau, engineering & marketing manager, Cylinder and Accumulator Division EuropeThis blog was contributed to by Erwan Jagueneau, engineering & marketing manager, Cylinder and Accumulator Division Europe (CADE).

 

 

 

 

Related, helpful content for you:

How to Specify the Proper Sized Heat Exchanger for Your Hydraulic System

Reduce Failure of Hydraulic Systems with Preventive Maintenance

Reliability Centered Maintenance Reduces Costly Downtime in Oil & Gas Applications 

Clean Hydraulic Fluids Are the Key to Top Performance 

A Dollars and Sense Approach to Preventing Hydraulic Oil Leaks

 

Categories
Recent posts by author

How to Select a Hydraulic Cylinder Accessory

How do I choose an accessory for an HMI, HMD or HMIX Series cylinder and why is the right accessory critical?   Cylinder mounting accessories and mountings transmit the force applied by a cylinder to...

Rail Vehicle Design Engineers Should Know This About EN 45545

The European standard EN 45545 was introduced in 2013 with a transitional period until 2016 and raises the level of requirements to the previous national standards, which have now been withdrawn. The...

Most Reliable Fitting for Rail: EO-2 Soft-Sealing Fitting for Leak-Tightness

The reliability of every component is significant for the design engineer of modern railway vehicles if they are to function smoothly in the long term. The EO-2 fitting has been extremely reliable for...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Note to Improve Hydraulic System Profitability with a Free Temperature Test Kit


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha