Parker United Kingdom

Nitrogen Generation: An Alternative to CO2 in Food-grade Applications

Fermentation factoryCarbon dioxide shortages this summer have caused production stoppages and restrictions for many UK food industry customers.

Breweries, food processors and packaging companies all experienced difficulties to varying degrees, following technical problems and maintenance closures at numerous CO2-producing plants across Europe.

Since then, many companies have started reviewing their supply chains to safeguard output in the event of any future shortfall in carbon dioxide production. And nitrogen generation is proving to be a commercially viable alternative to CO2 for multiple uses.

Food-grade nitrogen generation instead of CO2

Food-grade nitrogen is feasible as an alternative to carbon dioxide in a range of food and beverage applications, including:

  • Back-filling beer racking tanks
  • Counter-pressure filling of soft drinks  
  • Modified atmosphere packaging (also known as MAP, or ‘gas flushing’).

Within Europe, the European Industrial Gases Association (EIGA) has produced a specification that sets out the maximum contaminant levels acceptable for a gas to be considered food-grade. For example, nitrogen is given the additive number E941 when used in MAP applications.

Supply options

Typically, buying CO2 or liquid nitrogen in bulk requires some space for gas storage. There are also financial and environmental impacts associated with truck-based deliveries, as well as safety and handling responsibilities.

These days, however, it is also possible to generate food-grade nitrogen on demand - at a fraction of the cost of having gas bought in. This gives food producers the option to assume total control over their supplies and reduce operational costs significantly.

 

Nitrosource PSA nitrogen gas generators

Parker’s NITROSource PSA nitrogen gas generators are ideally suited to the challenges of modified atmosphere packaging (MAP), as well as specialist brewery applications such as sparging and kegging.

Even where carbon dioxide replacement is not feasible - for example, making drinks fizzy - nitrogen generation can partially offset usage and potentially help keep plants operating at full capacity with limited CO2 availability.

Also, the lower cost of generated nitrogen can help reduce expenditure and potentially reduce greenhouse gas emissions.

To find out more about how food-grade nitrogen can be used as an alternative to carbon dioxide, contact Parker’s United Kingdom team or visit http://solutions.parker.com/food-grade-nitrogen-for-breweries-food-and-drinks-packaging

 

 

 

Tony Brown - Parker Hannifin   This blog was contributed to by Tony Brown, sales manager (UK) Gas Generation

 

 

 

 

 

Related articles

Optimum Nitrogen Purity for Modified Atmosphere Food Packaging

Nitrogen: A Cost Effective Way to Extend Food Shelf Life

The Importance of a Food Grade Compliant Nitrogen Gas Supply

 

Categories
Recent posts by author

Corrosion: Types, Causes and Strategies to Prevent it

Corrosion management and prevention is a critical factor in many industrial settings. Left untreated, corrosion can put infrastructure, safety and business performance at risk – with potentially...

A LEAP to the Future: Leadership Program to Support Young Talent

In today’s competitive business environment, every company faces a major challenge: how best to attract, and keep, tomorrow’s leaders. Parker is staying a step ahead, by investing in an early...

Advanced Liquid Valves Expand Microfluidic Possibilities

Liquid valves are a critical component in the next generation of analytical equipment used for clinical diagnostics, analytical chemistry, environmental monitoring, agent detection, and other life...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Note to Nitrogen Generation: An Alternative to CO2 in Food-grade Applications


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha