Ray Clapp, owner of Coast Range Construction, Homer, Alaska, was searching for a way to increase efficiency on jobsites. In business for 16 years, Coast Range specializes in setting foundations for lodges and cabins as well as performing house-site development for contractors. Homer has very little flat ground to build on. Terrain ranges from sea level up to 1,400 feet in elevation, and drainage issues are quite common. On many jobsites, it is difficult to maneuver machinery, particularly in tight spaces. Machines often need to be moved several times during a job which can extend the time of a project. Additionally, the challenging terrain is often only accessible by water. Equipment has to be transported by barge. In order to differentiate himself from the competition, Clapp needed a tool that could easily work in tight spaces so that the work could be done cleaner and faster.
Clapp ultimately purchased the PowerTilt tilting coupler and added it to his Hitachi ZX200LC. With PowerTilt’s 180 degree side-to-side tilt and versatility, he can operate his Hitachi with surgical precision cutting all the slopes and angles with just one machine and without having to move it several times during the day.
“The PowerTilt is my secret weapon. It has increased the quality and efficiency of our work to give us the edge over the competition.”
Ray Clapp, owner, Coast Range Construction
PowerTilt uses an innovative sliding-spline operating technology to convert linear piston motion into powerful shaft rotation. Each actuator is composed of a housing and two moving parts – the central shaft and piston. As hydraulic pressure is applied, the piston is displaced axially, while the helical gearing on the piston OD and housing’s ring gear cause the simultaneous rotation of the piston. PowerTilt’s end caps, seals and bearings all work in tandem to keep debris and other contaminants out of the inner workings of the actuator, prolonging product life and reducing required maintenance.
The PowerTilt can be used with a variety of attachments. Coast Range mainly uses it for grading projects but some projects have seen the need to attach standard or narrow buckets.
Coast Range used to require three machines for any given project: the Hitachi excavator, a track loader and a small dozer. By adding the PowerTilt to his excavator, projects were completed one to two days faster. The small dozer was only being used an average of 90 hours a year where most machines average about 2,000 hours a year. Clapp estimates a 30 percent increase in productivity with the use of this tool. He also decided to eliminate the small dozer, and now saves one third of the time to complete the same work he used to do with the small dozer. Reduction in equipment decreases transportation costs too.
Purchasing the PowerTilt has given Ray an advantage over the competitors in the area by increasing productivity and creating a clean and more precise finished look on the jobsite. In using this tool for the past 10 years he has had no maintenance issues or downtime.
The PowerTilt is reliable. The PowerTilt has outlasted Clapp’s machinery. Regular scheduled maintenance and greasing have been key but ten years later, Coast Range’s current PowerTilt has up to 8,000 hours on it and is still going strong with no maintenance issues. Clapp has a lot of confidence that the PowerTilt will always finish the job in any type of weather, terrain or environment in Alaska.
PowerTilt is available for equipment up to 75,000 lbs in eight sizes with standard rotation of up to 180 degrees. Each model is designed for a specific class of machinery and individually customized to fit the carrier.
More product information can be found on PowerTilt here.
This article was contributed by Jessica Howisey, marketing communications manager, Helac Business Unit, Cylinder Division.
Related articles:
Lifters Designed with Rotary Actuators Dump Waste More Effectively
Essential Criteria for Selecting the Right Motor for your Hydraulic Application
Load Sensing Valve Improves Heavy Duty Machine Productivity and Fuel Savings
Have a question about Parker products or services? We can help: Contact Us!
Comments for Unique Tilting Coupler Technology Gives Construction Firm Competitive Edge
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.