Gas Generation

Using Nitrogen in the Plastics Industry

Using Nitrogen in the Plastics IndustryNitrogen is widely used in the plastics industry. Injection molding, film extrusion, and gas assist injection molding all use nitrogen because of its inertness and dryness. On site nitrogen is an ideal choice, as nitrogen can be generated on demand without relying on deliveries from a third party supplier.

In injection molding, moisture and oxygen can cause issues with the final product including defects and blemishes. Using dry nitrogen generated from a Parker on site nitrogen generator eliminates these complications.

Gas assist injection molding (GIAM) involves a multi-step molding process. It is a way to make thick plastic parts without issues created from excess shrinkage of the part. It is a type of injection molding that uses an inert gas to create a very dense and strong plastic part that uses nitrogen to pack out the part and compensate for shrinkage. First the polymer is injected into a mold though not all filled. Nitrogen under high pressure is injected into the polymer, pushing it into areas of the mold that are not yet filled. The nitrogen pressure is maintained during the cooling phase of the molding process, and gas pressure is released and the part is ejected. 

 

Using Nitrogen in the Plastics IndustryFilm extrusion is achieved by extruding a molten thermoplastic using a screw through a die. Afterward, it is inflated to many times its initial diameter forming a thin tubular film. Screw carbonization and frequent die cleaning, caused by oxygen in the feed throat hopper, are issues with blown film extrusion that can be improved or eliminated by using a nitrogen purge

To learn more about in-house nitrogen generation for the above applications, please call (800) 343-4048 or visit our product page for nitrogen generators.

We will help you size a system to meet your needs.

 

 

 

 

 

 

 

 

This post was contributed by David Connaughton, Nitrogen Generation Systems Product Manager, and Jennifer Fiorello, Gas Generation Technology Blog Team Member - Parker Hannifin

 

 

Related articles on this blog:

How Common is Nitrogen Generation?

How to Select an On-Site Nitrogen Generator

Top Frequently Asked Questions About Nitrogen Generators

Categories
Recent Posts by Author

Nitrogen Generation System Reduces Costs in Additive Manufacturing

Additive manufacturing or 3D printing is a relatively new rapid manufacturing technology that has become mainstream in recent years. It covers a wide variety of processes used to produce a multitude...

Energy-Saving Nitrogen Generator Prevents Gas Supply Disruptions

When it comes to supplying dry, inert nitrogen for manufacturing applications, there’s a lot more to PSA technology (pressure swing adsorption) nitrogen generators than vessels filled with CMS (carbon...

A Safety Plan for Compressed Gases in the Laboratory

Using compressed gases in the laboratory can be a dangerous situation if they are handled improperly. Many gases can be explosive, flammable, corrosive, and toxic. Because the gases are under high...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Using Nitrogen in the Plastics Industry


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha