Using a variable frequency drive (VFD) can be beneficial in many constant speed applications driven by electric motors, such as those that require controlled starting and have been historically served by a reduced voltage soft-starter (RVSS). While an RVSS and a VFD can both provide a controlled start, let’s examine the benefits of each technology and when it makes sense to use one over the other.
To learn more details about when to use a VFD in place of an RVSS, download the full white paper.
The differences between RVSS and VFDs and when to select one or the other for an application is determined by the following factors (when using a NEMA design B three phase induction motor):

An RVSS can be used to limit inrush current and reduce mechanical stresses on the motor and device it is powering during the starting cycle. The RVSS ramps the starting voltage from 40% (typical) to 100% over a set time (2 - 15 seconds typical). Starting torque is significantly reduced, rising to full torque at rated voltage.
By using an RVSS, locked rotor torque will be approximately:
Rated Torque x 2 x (% applied voltage)2
At a 40% start voltage, locked rotor torque will be:
Locked Rotor Torque = Rated Torque x 2 x (0.40)2 = 0.32 (32% of rated torque)
Because both the voltage and frequency are varied with a VFD, the motor will be at 100% flux at any speed resulting in the ability to produce 100% torque at 100% current at any speed below base speed. Therefore, a VFD can be used as a full torque soft starter in place of an RVSS. When used in this capacity, a VFD is capable of starting loads that require up to 200% torque such as mixers and production machinery with no inrush current.
Parker has recently introduced the AC10 series of general purpose VFDs, available at 230V to 20HP and 460V to 250HP and offer:
To learn more about Parker's VFD products, please visit our website.
Article contributed by Bill Riley, business development manager for the Drives Business Unit, Electromechanical & Drives Division North America, Parker Hannifin Corporation.
Ten Dos and Don'ts of Applying Variable Speed Drives to Hydraulic Pumps
VFD Slashes Wastewater Treatment Plant’s Energy Costs
5 Reasons to Control your Compressor with a Variable Frequency Drive
Have a question about Parker products or services? We can help: Contact Us!
Comments for Variable Frequency Drives Benefit Constant Speed Applications
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.