Webinars
Time to Inspect and Service Your Combustion Turbine Valves
Diminishing functionality of combustion turbine components due to aging parts is a concern for plant and maintenance managers. The harmonization of each individual part of a machine is crucial...
Read More ►
Challenges of Commercial Vehicle Electrification
In 1933, Kenworth Motor Truck Co. became the first American truck manufacturer to introduce the Cummins 4 cylinder, 100 hp, HA4 model diesel engine as standard equipment. By 1938 the first...
Read More ►
EMI Shielding Honeycomb Air Vent Panel Design Features
Honeycomb air vent panels are used to help cool electronics with airflow and while maintaining electromagnetic interference (EM) shielding. Recently, our team of experts held a webinar on...
Read More ►
Continuous Improvement Earns Aerospace Top Scores for Customer Service
For over a century Parker Aerospace has been an aerospace industry leader both as an original equipment manufacturer (OEM) and provider of aftermarket repair, maintenance, and overhaul (MRO) services....
Read More ►
How a Self-Retaining Static Seal Efficiently Seals Bores in Non-Pressurized Applications
What can be done if a bore requires radial sealing but lack of a lead-in chamfer prevents the installation of a seal? A situation like this occurs for instance when an existing bore should be closed...
Read More ►
How Tailored Single-Use Fluid Management Systems Benefit Biopharma Manufacturers
As well as pharmaceutical production based on complex organic molecules, manufacturing of advanced biologic drugs and vaccines must ensure that in-process contamination risks are mitigated...
Read More ►
Selecting a Thermal Gel or Thermal Gap Pad – Your Questions Answered (Part II)
This is the second part in a two-part blog post series answering the questions you asked during the webinar Selecting a Thermal Gel or Thermal Gap Pad now, available on-demand. Missed part 1? View it...
Read More ►
Selecting a Thermal Gel or Thermal Gap Pad – Your Questions Answered (Part I)
This is the first part in a two-part blog post series answering the questions you asked during the webinar Selecting a Thermal Gel or Thermal Gap Pad now, available on-demand. The objective of thermal...
Read More ►
Sterilization of Cell Culture Media - Taking on the Challenges
Cell culture media is a key component of upstream bioprocessing needed to encourage the growth and survival of cells. This is vital to achieving a viable cell density and, ultimately, the...
Read More ►
Reduce Downtime and Costly Seal Replacements: Seal Failure Diagnosis Part 2
As mentioned in part one of our seal failure blog series, O-ring and seal failures are often due to a combination of failure modes, making root cause difficult to uncover. It's important to gather...
Read More ►
Reduce Downtime and Costly Seal Replacements: Seal Failure Diagnosis Part 1
There are many situations where an O-Ring may not last as long as one thinks that it should. When the expectation is realistic and yet the seal fails earlier than expected, the...
Read More ►
Tackling the Source of Mycoplasma Contamination in Biopharmaceutical Processes
Mycoplasma contamination can have a devastating effect on drug manufacturers but what are the factors make a bioprocess vulnerable to Mycoplasma contamination and what measures can be put in place to...
Read More ►
Early Adoption Single-Use Technology Can Ensure Successful Process Scale-Up
Whether you are running a process in a 30,000 L bioreactor in fed-batch mode, a 200 L continuous process, or have scaled-out (rather than up), you will start at small scale and look to increase the...
Read More ►
A Guide to Biopharmaceutical Filter Qualification
Filter qualification typically involves demonstrating bacterial retention of a filter under process simulated conditions. A crucial first step in this is in the hands of the filter vendor, who...
Read More ►
Mycoplasma Contamination: Understanding the Risks and Taking on the Challenges
Mycoplasma contamination events, although rare, can have an enormous and immediate negative impact on biomanufacturers leading to reduced productivity and delays in products reaching patients. Parker...
Read More ►
How VFD Technology on Hydraulic Power Units Helps Improve Performance | Case Study
Combining electronic and hydraulic technologies can add efficiency and functionality to machinery and processes that use hydraulic pressure to operate. The hydraulic power unit (HPU), a workhorse...
Read More ►
The Benefits of Changing Your Microbial Stabilisation Process to Sterile Filtration
Brewers who wish to reach their sustainability goals - and produce more stable, fresher beer - should consider embracing a technology which is changing the face of the brewing industry. New...
Read More ►
Protecting Your Bioprocess From the Risk of Human Error
In Parker Bioscience’s webinar entitled Protect The Process, Protect The Patient, the concern that biopharmaceutical manufacturers have regarding the impact of human error on their processes was all...
Read More ►
A Guide to Business Continuity Planning for Biomanufacturers
Picture the scene: Unprecedented rainfall and poor flood defences causes flooding to a biopharmaceutical facility, damaging equipment, making large areas of a site unsafe and inaccessible, and...
Read More ►
Protecting Your Process From Mycoplasma Contamination
Plant shutdown, a shortage of key products, patients unable to access important drugs, profits hit … the consequences of a biological contamination can be devastating for a...
Read More ►