Compressed Air Gas Treatment

What are the Risks of Contaminated Compressed Air in a Food Plant? Part 2 of 6

Many types of bacteria can be present in compressed airKnowing the risks of compressed air contamination in a food processing plant is important.  Air is not as clean as it appears to be.  Untreated compressed air contains many potentially harmful or dangerous contaminants which must be removed, or reduced to acceptable levels, in order to protect the consumer and provide a safe and cost effective production process.  Along with moisture and particulate matter, inlet air to a compressor generally carries 5 to 50 bacteria per ft³.  Therefore, a 75 hp compressor with a capacity of 300 SCFM  takes in 100,000 to 1 million bacteria each hour.  These bacteria are compressed along with the air and begin their journey through the compressed air system.  Introducing this type of microbial contamination to food products is very risky and would be considered a lack of control by the facility.  Understanding how to operationalize the treatment of compressed air in a food production facility will help ward off that risk.

Where Compressed Air Contacts the Food

Sometimes it is not apparent where the compressed air is contacting the food.  Working surfaces like counters and conveyors are obvious and manageable contact points.  However, compressed air is invisible and leaves no visible trace of where it contacts the food, other food contact surfaces or the packaging.  Without adequate hurdles and physical barriers in place the microbial, particulate, and (in some cases) compressor oil contamination is left behind after the air dissipates.

Examples of processes that provide direct and indirect contact points are:

• Bagging

• Sparging/Mixing

• Drying

• Air Knives

• Pneumatic Exhaust (i.e., cylinder exhaust)

The image below shows a typical air knife application.

Image of air knife application

 

 

 

 

 

 

 

 

 

Read White Paper that benchmarks the current Good Manufacturing Practices from the most popular food safety standards and consolidates them into one easy to understand the document.

 

This is Part 2 of a 6 Part series on Compressed Air Contamination in Food Plants. Below are links to the rest of the series.

Are you Ready for an Audit? Is your Plant Compressed Air in Compliance with GFSI, SQF, and BRC Codes? Part 1 of 6

How to Manage the Risks of Food Product Contamination from Compressed Air. Part 3 of 6

Is Your Food Product Safe from Microbial Contamination? Part 4 of 6 

Understanding Good Manufacturing Practices for Compressed Air in Food Plants. Part 5 of 6

 

What’s the Best Line of Defense against Microbial Contamination of Food? Part 6 of 6

 

This series was written by Lee Scott, Market Development Manager, Parker Hannifin

Categories
Recent Posts by Author

Why Should I Change My Compressed Air Filter Element?

Often nicknamed manufacturing’s fourth utility alongside electricity, gas and water, compressed air is used in over 90% of the world’s manufacturing facilities. As with the other utilities, it is a...

How Oil Vapour in Ambient Air Affects Compressed Air Quality

Many companies, including those in the food and beverage, pharmaceutical, cosmetics, manufacturing and electronics industries, recognize the negative effects on quality created by oil contact with...

The Importance of Maintaining CO2 Gas Quality in Bottling Applications | Case Study

  Snap open a bottle of soda or beer and you will see, hear and feel the familiar fizz and bubbles. These sensations are the result of carbon dioxide (CO2), a colorless, odorless, non-combustible gas....
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for What are the Risks of Contaminated Compressed Air in a Food Plant? Part 2 of 6


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha