Sealing Shielding

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

what to know about o-ring cytotoxicity and the pharmaceutical industry, o-ring, oring, o ring, medical device sealsMost pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed to any cytotoxic contaminants that may leach out of the seals. It is also imperative that cytotoxic contaminants not be present in the finished drug, especially for infants, and for patients who are pregnant or nursing.

 

Cytotoxicity O-ring testing

Before an O-ring is approved for the pharmaceutical industry, it needs to be tested for cytotoxicity (cell toxicity). This is usually tested in the United States per USP <87>, and internationally per ISO 10993-5. These two tests are very similar in methodology and criteria. Both cytotoxicity tests use L-929 mouse fibroblast cells, which are an industry-standard cell used for cytotoxicity testing. Cultures of these cells are produced in glass flasks prior to testing. Extracts are prepared using 3 test articles: the O-ring material, a negative control article (HDPE), and a positive control article (PVC for USP <87>, and powder-free latex gloves for ISO 10993-5). These extracts are then added to the cell cultures. Cells are incubated with the extracts and then examined after 48 hours. The grading scale is from 0 to 4, with 0 meaning cells are completely unaffected, and 4 meaning all cells are destroyed. For the test to be valid, the HDPE extract must have a grade of 0, and the PVC extract must have a grade of 3 or 4. The O-ring material meets the requirements if the biological response is less than or equal to grade 2. Materials that pass the requirements of USP <87> or ISO 10993-5 are generally considered non-toxic to cells.

Parker offers several O-ring compounds that have been tested for cytotoxicity. 

USP <87> Approved ISO 10993-5 Approval
Ethylene Propylene (EPDM) Ethylene Propylene (EPDM)
E1244-70 E1244-70
E3609-70 E3609-70
E0740-75  
Silicone (VMQ)  
S1138-70  
SM355-75  
Perfluoroelastomer (FFKM)  
FF580-75  
  Fluorocarbon (FKM)
  V1274-80

If you have any questions or would like to learn more about O-ring Cytotoxicity testing, please feel free to contact Parker applications engineering or check out our interactive O-Ring eHandbook. You can also visit the Parker O-Ring & Engineered Seals Division website for more information.

 

MD&M WestPlanning to attend MD&M West 2020?

To learn more about Parker's solutions for medical and life sciences applications, stop by booth #1701 at Medical Device and Manufacturing West in Anaheim, February 11-13.

 

 

 

Perfluoroelastomer Materials Tailored for Your Needs

A Simple Guide to Selecting an O-Ring

Environmental Seal Enclosure 101

Have a question about Parker products or services? We can help: Contact Us!

Comments for What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha