Sealing Shielding

What You Should Know About Electrically Conductive Elastomers

What You Should Know About Electrically Conductive Elastomers - Elastomer Extrusion - Parker ChomericsElectrically conductive elastomers are elastomeric polymers filled with metal particles. They can be grouped by filler type and elastomer type. Then within each of these classes, there are standard materials and specialty materials.

Parker Chomerics manufacturers electrically conductive elastomer gaskets, also known as EMI elastomer gaskets, under the CHO-SEAL brand. We won't get so much into gasket configurations and dimensions here, we'll just stick to classes of materials. So what is available? Let’s find out.

Conductive elastomers are metallic particle filled elastomeric polymers, the particles giving the shielding performance and the polymer making them “rubber." There are many materials within this generic material type, but we'll focus on the below.
 

Particle fillers

Setting up the grades of conductive elastomers by filler types involves six different particles:

What You Should Know About Electrically Conductive Elastomers - Filler Types - Parker Chomerics

 

 

Three types of elastomer material

  • Silicone
    A polymer that has a large temperature range especially on the low end down to -55F. It is a very soft material with a low compression set. 
     
  • Fluorosilicone
    Close to silicone, but will not swell and degrade when exposed to solvents, fuels hydraulic fluids and other organic fluids. Although slightly harder than silicone, it is still relatively soft with low compression set properties.
     
  • Ethylene propylene diene monomer (EPDM)
    Does not have the temperature range nor the softness of silicone, but is resistant to highly chlorinated solvents used for compliance with NBC decontamination and is only used for applications with those needs.

All of these materials are cured or cross linked when the gasket is made. The cure either happens with heat or atmospheric moisture.
 

Three main processes used to process the material into a gasket

  • Compression molding - uncured material is placed into a mold that has a cavity machined into it. The mold is closed, put into a press, then with heat and pressure the material is formed into the gasket shape mirroring the cavity and cured with heat. This process is used for sheet stock also.
     
  • Injection molding - instead of hand loading the mold with approximately the proper amount of material, the mold is closed, then the proper amount of material is injected into the cavity. The process is much faster and because the right amount of material is injected tighter size tolerances can be obtained. Injection molding tooling is more expensive than compression molding.
     
  • Extrusion - raw material is pushed through a die with the cross section machined into it to create extruded cord stock. Heat is applied on the die and a finished continuous gasket strip is made. These gasket can be supplied in lengths or cut to size and then corners or intersections glued or spliced together to make a ready to use gasket.

In general, for small cross sectional electrically conductive elastomer shapes, the smaller the particle the more producible the part will be. Particle fillers have little to do with mechanical properties of the gasket except that they simply increase hardness.

Now that you have more information about how to select particle and polymers for electrically conductive gaskets, download or Electrically Conductive Elastomer Handbook and get started today!

What You Should Know About Electrically Conductive Elastomers - Conductive Elastomer Engineering Handbook - Parker Chomerics

 

 

 

 

 

 

 

 

 

Electrically Conductive Elastomer Particle Filler and Polymer Types - Jarrod Cohen - Parker Chomerics

 

 

This blog contributed by Jarrod Cohen, marketing communications manager, Chomerics Divison.

 

 

 

 

Related content

New Essential Handbook for EMI Shielding Applications

EMI Shielding Gaskets: Spliced Gaskets vs. Molded Gaskets

Can Electrical Resistance Be Used to Predict Shielding Effectiveness?

 

 

 

Have a question about Parker products or services? We can help: Contact Us!

Comments for What You Should Know About Electrically Conductive Elastomers


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha