Electromechanical

What You Should Know About Gearhead Sealing

Bacon Line - Food Processing, Getty Images - Parker HannifinApplications involving machines for gluing, fill, sealing and diverting of food containers for the food processing industry often use planetary gearheads. The motor and gearhead need to be mounted above the food plane. The gearheads often require modifications and proper sealing to make it safe in this environment, as well as making the gearhead able to withstand frequent washdowns.

Understanding gearhead sealing ratings

Do you want to understand more about gearhead sealing ratings? You’ve come to the right place. To start, gearheads are classified according to the International Protection Rating (IP Code) by the degree of protection the gearhead has against the intrusion of foreign matter. The first numeral designates the degree of protection the product has with respect to the ingress of solid objects. The second numeral designates the degree of protection the product has with respect to the ingress of water.

Sealing gearheads

Gearhead cutaway PS Gearheads - Parker Hannifin ElectromechanicalParker's helical planetary and bevel gearhead product lines (PS/PX/RS/RX/RB/RD/RT) are sealed to IP65 for complete protection against dust (dust tight) and washdown conditions (projection of water jets at a pressure of 30 kN/m^2 at a distance of 3 meters). Our PV gearheads are sealed to IP64 for complete protection against dust (dust tight) and splashing water. The spur NE product line is sealed to IP54 where ingress of dust is not totally prevented but will be fine on a machine where the ingress of dust will not be in sufficient quantity to interfere with the satisfactory operation of the machine. As with the PV product line, it is also protected against splashing water.

You must take these ratings into account when selecting a Parker gearhead for your application. Please contact us at c-parker@parker.com with your questions if you are unsure of your requirements, or if special requirements need to be taken into account.

 

Check out our video overview of planetary gearheads.


 

 

Jeff Nazzaro Product Manager ElectroMechanical NA Automation Group Parker HannifinArticle contributed by Jeff Nazzaro, gearhead and motor product manager, Electromechanical Automation North America


 

 

 

 

 

 

 

 

Other related posts:

When to Use Gearing in Motion-Control Designs Part 1 of 2

When to Use Gearing in Motion-Control Designs Part 2 of 2

GVM Motor Gives Traction to Brammo's Winning Motorcycles

Food Grade Gearhead Motor Solves Problem for Packaging Manufacturer

How Gearheads Reduce Inertial Mismatches Solving Design Challenges

 

Categories
Recent Posts by Author

Electromechanical and Drives Technology - A Look Back on 2019

Thanks to our loyal followers for all of the interest in the topics covered in this blog over the past year. In examining the most-read blog posts over the course of 2019, it becomes obvious that...

Time-Saving Solution for Servo Presses and Joining Applications

In industry, time is money. So, for engineers who are time-pressured, there is a solution for electromechanical press and joining applications. Push-To-Fit is an innovative electromechanical solution...

High-load Rodless Actuators Powering the Factory Automation Revolution

The arguments advocating more automation in our factories and process plants are gaining momentum and translating into a revolution in production environments.  Parker designs automated linear motion...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for What You Should Know About Gearhead Sealing


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha