Bioprocess Pharmaceutical Filtration

What's Stopping You From Automating Your Single-Use Process?

What's Stopping You From Automating Your Single-Use Process - Robot Pushing Button - Parker domnick hunter Process Filtration DivisionThe use of automation in running complex single-use systems has many benefits such as process control and consistency, increased speed, reduced labour costs and operational flexibility.

While implementation of automation is on the rise, perceived challenges around its adoption mean that its efficiencies remain untapped by some biopharmaceutical manufacturers.

Our recent webinar Single-Use Technologies, What is Next? provided an in-depth insight into the challenges faced by biopharmaceutical manufacturers when implementing single-use technologies.

Here we look at the points raised around introducing automation into single-use processes and focus on some of the perceived barriers to its implementation. 

Process Protection: What Does it Mean to You?_Webinar_Parker domnick hunter Process Filtration

 

Single-Use Technology, What's Next? 

Watch on Demand

 

 

In a poll taken during the webinar delivered by Graeme Proctor, Parker domnick hunter product manager for single-use technologies, 48% of respondents cited cost as being the main restriction to implementing automation. Though the initial outlay may appear costly, automation can provide rapid return on investment—in some cases as early as within one year—due to savings in labour cost and investment in facilities. In addition to the financial benefits, other efficiencies can also be achieved through automation.

What's Stopping You From Automating Your Single-Use Process?_Parker domnick hunter Process Filtration_Pie Chart1

Quality

Variation in a process implies that the product can no longer be assumed to be the same as that tested during clinical trials. This is where automation really comes into its own, adding great value and robustness to processes.

Four sources of process variation in biopharmaceutical manufacturing are biological, raw materials and consumables, operational input and environment (namely temperature and contamination). Automation can help by increasing process consistency and eliminating variation derived from operational and environmental inputs.

 

Streamlined processes

Automation can offer a huge number of improvements to single-use processes. It can free up the operator, allowing safe and effective multitasking while ensuring the safety of processes and products.

Processes such as normal flow filtration (NFF), tangential-flow filtration (TFF), bulk final fill and chromatography are all historically labour-intensive, manual operations. In another poll taken during the webinar, 38.5% of respondents thought that final bulk fill is the unit of operation that would benefit most from automation, closely followed by chromatography with 34.6% of the votes.

 

What's Stopping You From Automating Your Single-Use Process - Pie Chart 2 - Parker domnick hunter Process Filtration Division

In addition to providing a faster, safer final bulk filling process which virtually eliminates the chance of cross contamination, automation can provide standardization from start to finish—giving control of pressure, monitoring and feedback on parameters such as conductivity and temperature. Standard, reliable programming can also eliminate human error, ensuring a reliable and robust process.

Data acquisition and analysis can be automated and transcription error-free reports generated automatically, which in today’s fast-flowing market, is essential to ensuring compliance with 21 CFR Part 11 and GMP Standards.

Additionally, automation is also able to detect and reduce variation within processes and parameters which would be impossible to perform manually.

 

Conclusion

While Parker domnick hunter acknowledges that cost can be a stumbling block, automation can provide a complete solution, ensuring both the integrity and quality of the product while also significantly reducing the opportunity for errors and failures.

Automation can offer:

  • Rapid ROI
  • Time savings
  • Reduced complexity
  • Improved process security
  • Reduction in training requirements
  • Reduction in QA oversight

All of this adds up to a reliable and repeatable process that can simplify scheduling to enable a greater throughput with a lower cost of goods. 

Process Protection: What Does it Mean to You?_Webinar_Parker domnick hunter Process Filtration

 

Single-Use Technology, What's Next? 

Watch on Demand

 

 

 

What are the barriers to implementing automation in your single-use process? Let us know in the comments section below. 

 

What's Stopping You From Automating Your Single-Use Process? - Graeme Proctor, product manager - Parker domnick hunter Process Filtration DivisionThis post was contributed by Graeme Proctor, product manager - single-use technologies, Parker Bioscience Division, United Kingdom.

 

Parker Bioscience Division Specializes in automating and controlling single-use bioprocesses. By integrating sensory and automation technology into a process, a manufacturer can control the fluid more effectively, ensuring the quality of the final product. Find out more at www.parker.com/bioscience

 

Related Content

Four Sources of Process Variation in Biopharmaceutical Manufacturing

Automation of Final Bulk Filtration and Container Fill Step in GMP Environment 

A Strategy for Avoiding Manual Errors in Biomanufacturing

10 Things to Consider When Assessing Your Single-Use Bioprocess Automation Requirements

How to Successfully Scale-Up Automated Single-Use Bioprocesses

 

Categories
Recent Posts by Author

Listening, Learning and Applying Knowledge in Product Development

Although bulk filtration of a product prior to shipping was one of the first bioprocessing steps to benefit from single-use technology, it has been one of the last to benefit from...

Early Adoption Single-Use Technology Can Ensure Successful Process Scale-Up

Whether you are running a process in a 30,000 L bioreactor in fed-batch mode, a 200 L continuous process, or have scaled-out (rather than up), you will start at small scale and look to increase the...

Making Connections? Make the Right Choice for Your Single-Use Process

Single-use solutions have been widely adopted on a global scale within the biopharmaceutical industry due to the many advantages and process improvements they offer. Key applications for single-use...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for What's Stopping You From Automating Your Single-Use Process?


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha