Sealing Shielding

When the Heat is Turned up on Your Polyurethane Seals, Consider Resilon® 4350

When the Heat is Turned Up On Your Polyurethane Seals, Consider Resilon 4350, Engineered Polymer Systems Division, Resilon 4350Have you had problems with your polyurethane seals degrading, especially when exposed to higher heat creating the need to replace your seals more often than you would like? As you probably know, seal replacement creates costly downtime that can be avoided if you have an appropriate seal for the job. Parker's Resilon® 4350 polyurethane is up for this task. Resilon 4350 is designed for sealing at higher temperatures up to 250°F continuous and can withstand short-term excursions of up to 300°F without leakage. 

 

Understanding the approximate temperature range of Resilon 4350

Resilon 4350 polyurethane was formulated to extend the high-temperature capability of Parker’s proprietary urethanes. Where current, more ordinary polyurethane seals have failed, Parker’s new Resilon 4350 has the highest temperature rating of any specialty polyurethane on the market. It was developed for applications where high temperatures or extended heat history cause failures with current polyurethane seal materials.

In a head-to-head comparison test at 250°F continuous, the Resilon 4350 material presented minimal leakage (< 5 grams) up to 250,000 cycles during a life test. This equates to a 33% longer lifespan compared to the standard 4300 material at this elevated temperature range (Figure 1).

When the Heat is turned up on your polyurethane seals, consider resilon 4350, engineered polymer systems division, resilon 4350Additional testing was completed showing the % seal force retention as the external temperature increased from about 160°F to 250°F. The three materials tested exhibited a linear relationship between the seal force retention and temperature. The Resilon 4350 had a 7-10% higher seal force retention beyond 4300 and the leading competitor of high-temperature polyurethane during this temperature range. The Resilon 4350 still exhibited a 20% seal force retention at 250°F (see Figure 2). Based on the results of this testing, this material is promoted as having a continuous operating temperature range of -65°F to 250°F.

Parker’s Resilon polyurethanes are provided in various profiles for use in a wide variety of applications. With the introduction of Resilon® 4350 the recommended operating temperature range for best performance can now be extended 20° to 25°F higher, giving design engineers the ability to push the envelope.

Follow this link to learn more about Resilon® 4350 and Parker's other Polyurethane 4300 formulations

 

IFPE 2020Planning on attending IFPE 2020?

To learn more about Parker's off-road machinery solutions, stop by booth #S80245 at IFPE/CONEXPO-Con/AGG in Las Vegas, March 10-14.

 

When the heat is turned up on your polyurethane seals, consider resilon 4350, engineered polymer systems division, resilon 4350

 

This article was contributed by Eric Woodworth, application engineer, Engineered Polymer Systems Division

 

 

 

 

Related content: 

Thermal Capabilities & Polyurethane Seal Materials: What Do Temperature Ratings Mean?

High Performance Seals for Extreme Aerospace Environments

Medical Polyurethanes for Life Science Applications

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for When the Heat is Turned up on Your Polyurethane Seals, Consider Resilon® 4350


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha