Electromechanical

When to Use Gearing in Motion-Control Designs Part 2 of 2

Electromechanical processing packaging plant - gearmotors gearheads The appropriate use of gearing in your motion control application can make it run at lower rpms and provide more torque. Should you decide to use a gearhead, available configurations include an in-line or a right-angle gearhead. You must and also decide whether you want a motor with an integrated gearhead. The assembly includes both the gearhead and motor in a single housing.

Types of gearheads

In-line gearheads

In-line gearheads are commonly used for motion control applications because they have higher torque output and lower backlash than right-angle gearheads. They also cost less. In-line gearheads have an output shaft that is in line and centered with the motor shaft. 

Right angle gearhead

right angle gearhead  Parker Hannifin - Bayside Electromechanical North American DivisionA right angle gearhead is commonly used when it’s necessary to fit a servo motor into a tight space. The output shaft of the right angle gearhead is at a 90-degree angle to the motor shaft.  Therefore, most of the gearhead housing, and all of the motor housing, is parallel to the side of the machine, providing a smaller machine envelope. Note that some gearheads, such as worm gearheads, have an inherent right angle design because the drive axis of the worm (screw) is at a 90 degree angle to the axis of the worm gear.

Fig 1. A right-angle gearhead such as this is commonly used when it is necessary to fit a servo motor into a tight space

Separate motors and gearheads

Most motion control systems that employ gearing use separate motors and gearheads. This approach lets you choose the motor and gearhead most appropriate for the application, even when they come from different manufacturers. Typically, you can mount gearheads to just about any servo motor. All that is required is to mount the mating flanges together using standard screws. This configuration is more flexible than an integrated gearmotor and it’s easier to maintain. Gearheads wear out more quickly than the motor itself, so when a gearhead fails, you only have to replace it and not the motor.

Integrated gearmotors

That said, an integrated gearmotor is the best choice for certain applications. One advantage of this approach is the overall length of the assembly can be an inch or more shorter than an assembly with a separate gearhead and motor.

System design is simpler too because you only need a single speed and torque curve to determine if a gearmotor will provide the necessary performance to power your motion control system. This helps eliminate design errors.

And assembly is simpler as well. Because the gearhead and motor are integrated, it’s impossible make the assembly mistakes found when mounting a gearhead to a motor. 

Use in food processing

Integrated gearmotors work well in harsh environments such as found in the food processing industry. Because gearmotor housings are also made with 300 grade stainless steel and must meet IP 69K standards for resistance to the ingress of high temperature-high pressure water, plant personnel can easily wash down machinery without having to worry about harming it. The design also eliminates the seam between the motor and the gearhead, so there is no place for food to get caught.

Flange-face gearheads

Mating Flange Parker Hannifin To mount a gearhead to a servo motor, all that is required is to attach the mating flanges together using standard screws. Here, a split collar mechanism on the input gear secures it to the motor shaft.A newer trend is the use of flange-face gearheads. Instead of an output shaft, flange-face gearheads have a rotating disk with screw holes on the output. The machine being driven mounts directly to the flange. This arrangement eliminates the need for a flexible couple and all of its associated problems. Both gearheads and gearmotors are available with a flange face.

Fig 2. To mount a gearhead to a servo motor, all that is required is to attach the mating flanges together using standard screws. Here, a split collar mechanism on the input gear secures it to the motor shaft.

Choosing the right gearhead

There are many different types of gearheads for use in a motion control system. Knowing the attributes of each will help you make the best choice for different applications:

  • Spur gears have teeth that run perpendicular to the face of the gear. They are compact, cost-effective, and capable of high gear ratios. Disadvantages include they are noisy and prone to wear.
  • Worm gear drives are used where it’s necessary to transmit power at a 90-degree angle and where high reductions are needed. Worm drives are precise, run quietly, and need little maintenance. Disadvantages include they are relatively low in efficiency and are non-reversible.
  • Planetary gear drives are so called because the gear arrangement somewhat resembles the solar system. A central gear, called the sun gear, drives planetary gears positioned around it. The planetary gears rotate the output shaft of the gearhead. Advantages include compact size, high efficiency, low backlash, and a high torque to weight ratio. Disadvantages include complex design and high bearing loads.
  • Harmonic gear drives contain a wave generator, flexispine, and circular spine. Advantages include low weight, compact design, no backlash, high gear ratios, high torque capability, and coaxial input and output. A disadvantage is the gears are prone to wear.
  • Cycloidal drives have an input shaft that drives an eccectric bearing which then drives a cycloidal disk. Cycloidal speed reducers are capable of high ratios while remaining small in size. Disadvantages include increased vibration, caused by the cycloidal motion, which can cause wear on the cycloidal disk’s teeth.

Parker Hannifin Gearmotor. You only need a single speed and torque curve to determine if an integrated gearmotor such as this has the necessary performance to power the motion-control system.  Fig 3. You only need a single speed and torque curve to determine if an integrated gearmotor such as this has the necessary performance to power the motion-control system. 

 

For more information, on the range of gearheads and gearmotors for use in your design see Parker's Electronmechnical Division page

 

This is Part 2 of a 2 Part series shared by Jeff Nazzaro, Gearhead and Motor Product Manager, Parker Hannifin - Electromechanical North America Division

 

See Part 1 - When to Use Gearing in Motion-Control Designs Part 1 of 2

Categories
Recent Posts by Author

Electromechanical and Drives Technology - A Look Back on 2019

Thanks to our loyal followers for all of the interest in the topics covered in this blog over the past year. In examining the most-read blog posts over the course of 2019, it becomes obvious that...

Time-Saving Solution for Servo Presses and Joining Applications

In industry, time is money. So, for engineers who are time-pressured, there is a solution for electromechanical press and joining applications. Push-To-Fit is an innovative electromechanical solution...

High-load Rodless Actuators Powering the Factory Automation Revolution

The arguments advocating more automation in our factories and process plants are gaining momentum and translating into a revolution in production environments.  Parker designs automated linear motion...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for When to Use Gearing in Motion-Control Designs Part 2 of 2


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha