Fluid Gas Handling

Why are Brass Fittings Preferred by Truck Manufacturers?

Why do Truck OEMs Use Brass Fittings Like many industrial markets, the heavy truck market utilizes brass fittings for a variety of applications. With composite fittings gaining traction in the arena, why do many truck OEMs continue to use brass fittings? 

 

Why is brass the ideal material for the transportation market?

Like many industrial markets, the heavy truck and transportation markets utilize brass fittings for a variety of applications. Brass fittings have the strength, corrosion resistance and machinability in a variety of shapes and sizes to provide cost-effective solutions; making them an ideal material for many truck applications. It is common to find brass fittings in the air brake systems, cab controls, fuel systems, engine, transmission, cooling and air tanks on a heavy-duty truck and they meet DOT and SAE requirements. Let’s take a deeper look into why brass is an ideal material for this market.

 

Why do Truck OEMs Use Brass Fittings - brass fittings in debur machine - Parker Fluid Systems Connectors Division Brass is comprised of approximately 60 percent copper, 38 percent zinc, and 2 percent lead. Brass fittings are characterized by their strength and ability to handle high as well as reasonably cold temperatures. They have good conductivity, excellent corrosion resistance, and low magnetic permeability. Brass not only is easy to machine, but it has great plating, joining, polishing and finishing characteristics all packed into a relatively low cost material for manufacturing.

 

 

 

How are brass fittings manufactured?

Why do Truck OEMs Use Brass Fittings? - Bar stock of brass - Parker Fluid System Connectors Division

In manufacturing, there are two methods for creating a brass fitting, one from extruded bar stock and the other through forging. A fitting made from extruded bar stock is created from bar stock in round, hexagon or shaped bars. These bars began as a solid round billet that is heated to a pliable state and forced by approximately 80,000 pounds of pressure through a die resulting in a bar, shaped to the desired external dimensions. That bar is then cut into slugs and machined into fitting components. The process produces a dense, nonporous material.

A forged fitting is made from an extruded round bar that is cut to length and straightened. After straightening, the bars are cut into slugs, much like a fitting from extruded bar stock, but at this point, rather than machining, the slugs are reheated to a pliable state and pressed under approximately 25,000 pounds of pressure per square inch between an upper and lower die cavity into the desired fitting shape. After cooling, the flash, or excess, is trimmed away and the forging blank is ready for machining.

Why do Truck OEMs Use Brass Fittings - Machining Brass infographic - Fluid System Connectors Division Parker Hannifin The forged fittings produce a uniformly dense material of exceptional strength from forming under extreme pressure. Since the grain flow follows the contour of the fitting shape, the fitting has high impact strength and resistance to mechanical shock and vibration. You can easily spot the difference between a forging and an extruded part by looking at it. A forging will have rounded edges characteristics of the forged shape from the die and an extruded part will have squared off corners that resemble the original bar stock they originated from. Brass fittings can have components from both manufacturing methods that are assembled together to create a finished part.

 "Brass compression style fittings, which have been used in the industry for decades, remain a low-cost fitting option for truck and trailer OEMs."  Tom Cook, product sales manager, Fluid System Connectors Division, Parker. 

Some applications, like diesel fuel applications, require additional corrosion resistance above and beyond the capabilities of brass alone. The great plating characteristics of brass, allow nickel-plating to original brass fittings to accommodate fuel systems.

Parker’s Fluid System Connectors Division offers the widest range of brass fittings for the transportation market. From extruded, forged, plated, and even composite materials, we make connections to bring increased efficiencies and higher productivity. Our vast offering of NTA, Transmission, Vibra-Lok, Prestomatic, PTC, Air Brake Hose Ends and PMH and Pipe fittings can fit the needs of the heavy truck market with superior quality.

 

See how Parker is going the extra mile for the transportation industry. View the video now.  

 

 

For more information about our vast offering of transportation fittings, please visit our DOT Fittings Website or contact Parker Fluid System Connectors Division at (269) 694-9411.

 

Why do Truck OEMs Use Brass Fittings? - Samantha Smith - Marketing Services Manager - Fluid Systems Connectors Division Article contributed by Samantha Smith, marketing services manager, Fluid System Connectors Division

 

 

 

 

 

Additional articles from out Fluid and Gas Handling Technology team:

Metallurgy Makes or Breaks Tube Fittings

The Truth About Pressure Ratings for Hydraulic Fittings and Adapters

Choosing the Right Connector, Tubing and Accessories for Your Application - Part 1

 

Categories
Recent Posts by Author

How Condition Monitoring Can Transform the Food and Beverage Industry

Our sense of taste is changing. We’re becoming more health conscious of the foods and beverages we consume to living a better life. No more perplexing and hard-to-pronounce food labels....

Frequently Asked Questions About Seal-Lok for CNG Fittings

Seal-Lok for CNG Fittings and Adapters provide reliable natural gas fuel conveyance in CNG applications with an O-ring face seal design that incorporates an elastomeric seal compound made of...

Any pressure. Any project. One solution. Infographic

GlobalCore is the future that OEMs and end users around the world have been asking for: a unified family of robust hydraulic hoses designed to endure the tough conditions where work gets...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Why are Brass Fittings Preferred by Truck Manufacturers?


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha