Sealing Shielding

Why is Shore A Hardness Important?

Shore A Hardness Testing on O-ring - Parker HannifinO-rings are the simplest, most readily available type of seal used across every industry and market. They are arguably the best seal for many applications, but perhaps daunting to an engineer with no experience in seal design. The O-Ring Basics chapter of Parker's eHandbook provides an overview of what an O-ring is, how it works, and finally, the benefits over other seals.

One very important consideration is the hardness of a rubber material. A customer may need to seal a high pressure fluid, which would call for a harder material. On the other hand, he might want to minimize insertion force, or the O-ring may be sealing some delicate hardware, such as thin plastic or a sapphire plate. This may call for a softer material. For testing the hardness of the material, Parker recommends Shore A hardness. It is an industry standard test for rubber, and it is an acceptance criteria for every batch of O-ring material mixed by Parker.

What is Shore A hardness and how is it tested?

Shore A hardness testing is performed using a durometer, which was developed by Albert Ferdinand Shore in the 1920’s. The Shore A hardness measurement is often colloquially called “durometer” or “duro”. This test is performed on cured rubber sheets per ASTM D2240, and on finished O-rings per ASTM D1414. 

The device consists of a hardened steel rod with a truncated cone at the tip. The steel rod is spring-loaded and actuates a dial with a scale of 0 to 100. The test specimen is placed directly underneath the truncated cone, and the device is pressed down onto the part until the flat metal plate on the bottom is flush with the rubber specimen.

The more the cone deforms the rubber material, the lower the hardness measurement. The less the cone deforms the rubber material, the higher the hardness measurement.

How to read a Parker part number

Parker compounds utilize a distinct numbering system, which consists of one or two letters to designate material, a three or four digit identification number, and a two digit number for the Shore A hardness. Two examples of this are N0674-70 and NM304-75. Of particular interest are the last two digits, which indicate the nominal hardness of the material. Compound N0674-70 has a Shore A hardness of 70, while NM304-75 has a Shore A hardness of 75. The tolerance on the Shore A hardness is +/-5 for all Parker compounds.

For further information, check out the Material Selection Guide which provides a compound family overview including a description of compound advantages, typical temperature maximum/minimum, compatible fluids, and material durometers. A list of incompatible fluids are also detailed, allowing the user to receive a concise summary of the most common, and even the more obscure elastomer types. And check out the Parker O-Ring eHandbook or visit the Parker O-Ring Division for further information and useful tips on how to select an O-Ring. If you have any questions, please feel free to contact Parker applications engineering at 859-335-5125. 

 

David Mahlbacher

 

 

This article was contributed by

David Mahlbacher, Parker O-Ring Division, Applications Engineer

 

 

 

Other related blogs:

3 Guidelines to Ensure Proper Seal Installation

New O-Ring eHandbook Provides a Premier User Experience

Answers to Your In-Service Rubber Properties Questions

Avoid Seal Extrusion with a Robust Gland Design

Categories
Recent Posts by Author

How to Solve Large-Size Sealing Challenges at Temperatures up to 800 °C

When classic sealing materials – for instance in temperature ranges above 300°C and below -50°C – reach their limits alternative materials are required such as metal with appropriate coating/plating....

What to Know About O-Ring Cytotoxicity and the Pharmaceutical Industry

Most pharmaceutical manufacturers produce drugs in large vats of living cell cultures. For the production of these drugs, it is extremely important to ensure that these cell cultures are not exposed...

Five Things to Consider When Dispensing Form-In-Place EMI Gaskets and Thermal Gel

Automated form-in-place (FIP) dispensing of EMI shielding gaskets can be ideal for complicated patterns on electronics housings because automation allows for control over the size and shape of the...
Comments

Have a question about Parker products or services? We can help: Contact Us!

Comments for Why is Shore A Hardness Important?


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha