Small and mid-scale LNG plants are dramatically changing the application sphere for natural gas as an alternative fuel for transportation, both onland and for marine shipping use. They are helping drive adoption in various high horsepower applications and making gas capture and distribution from remote areas and wells without pipelines a reality.
As the requirement for small and mid-scale LNG plants grows, so does the need for tube connection technology for smaller line sizes. In the past, connection technology was limited to either orbital welding or double ferrule compression fittings. Today, driven by cryogenic applications, there are four connection options in the less than two-inch space: instrumentation compression double ferrule fittings; instrumentation compression single ferrule fittings; O-ring face seal fittings; and permanent fittings.
Connection in a cryogenic application should focus on five critical areas:
Safety is critical in small and mid-scale LNG plants. In these complex plants, electricity, gas and water will often coexist in close proximity. Add cryogenic temperatures to the mix and the environment becomes extreme.
The most important rule of safety in an LNG plant is to keep the media contained. Good tube connections prevent catastrophic failure at connection points. A failure mode and effect analysis reveal the threat that a bad connection – or a poorly made one – can pose to a plant. In addition to explosion leaks, the danger of frostbite exists with cryogenic temperatures. A good connection is a first defense in preventing exposure and harm to personnel.
Leakage of methane, a greenhouse gas -- while still not regulated -- is a major concern in LNG plants. Overall, fugitive emissions will become increasingly important; keeping hundreds and thousands of connections in an LNG plant from leaking will be key.
As a basic requirement, ensure bubble-tight connections that follow appropriate leak specifications to future-proof against fugitive emissions while not limiting solely to safe exposure levels. Apart from methane leaks, cryogenic fluid leaks can cause frostbite and major freezing hazards. A small, seemingly safe leak is also a loss of revenue and efficiency. Leak-tight connections can add up to savings and notable percentage points of efficiency.
A big challenge for small-scale, modular LNG plants is the flexibility to connect on-site to a dispensing system or a point-of-use system. This often means a lot of field connections and the capability to carry out repairs. Other times it means making certain connections at the time of installation. While welding sometimes seems to be the most straightforward strategy for a permanent joint, finding certified and trained welders may not be simple or easy.
With the operational life of an LNG plant in the range of 15 to 25 years or more, it is critical to select corrosion-resistant, robust and reliable connection technologies that outlast the moving parts. Longevity can be achieved by choosing materials that resist corrosion from environmental sources and that are compatible with the media or fluid being transported.
Finally, it is essential to consider applicable codes of construction that, in some environments, may include marine standards such as those for ABS or DNV GL. Code compliance helps ensure that all the above topics are covered. Codes to consider include:
The end-use must take into account all possible interface points such as vehicles, tankers, vessels or rail cars to define application standards.
In both single and double ferrule fittings, stainless steel parts that rub together under high pressure have a strong tendency to cold weld and seize, leaking to leaks and the resulting fugitive emissions.
Using fittings coated with molybdenum disulfide can avoid this problem. Solid molybdenum disulfide readily adheres to surfaces, is noted for its lubrication and anti-seizing properties, and does not squeeze out under extreme pressure. The result is low assembly torque and consistent, leak-free performance, even with repeated remakes.
Many fittings manufacturers also combat fitting leaks – and the resulting possibility of fugitive emissions – through proprietary ferrule-hardening processes designed to heighten corrosion resistance. For example, Parker treats its ASTM 316 stainless steel, single and double ferrule fittings with Suparcase®. The chemical process provides greater resistance to pitting, as well as excellent stress corrosion performance to provide longer, leak-free service life.
Article contributed by the Process Control Team. Original article published at LNG Industry in September 2015.
Related articles on Alternative fuels - CNG and LNG:
Transportation Fuel - LNG OR CNG?
How New LNG and Natural Gas Fuel System Architecture is Advancing the ‘Golden Age of Gas’
The Choice Between LNG and CNG as Transportation Fuel
Parker Complete Piping Solutions Receives ASME B31 Compliance
Is It Safe to Mix Compression Style Instrumentation Tube Fittings?
Manifold Connector Technology – Why Settle for Second-best?
How to Avoid H2S Embrittlement in Instrumentation Connections
Have a question about Parker products or services? We can help: Contact Us!
Comments for Why Making the Right Tube Connections for LNG Plants Is Vital
Please note that, in an effort to combat spam, comments with hyperlinks will not be published.