Aerospace

Elevating Flight With Decades-Strong Aerial Refueling Solutions

Elevating Flight With Decades-Strong Aerial Refueling Solutions- Aerial Refueling - Parker AerospaceWith an increased focus on strengthening United States military capabilities for the 21st century, Parker Aerospace takes pride in having a long history supporting the country’s defense endeavors around the world with flight-critical components. One of Parker’s most essential product lines for military aircraft is its aerial refueling equipment.  


In-flight refueling couplers, nozzles, receptacles, and test kits from Parker Aerospace’s Fluid Systems Division represent today’s leading edge in design, performance, and durability. 

Elevating Flight With Decades-Strong Aerial Refueling Solutions - Receptacle Stacks - Parker AerospaceThe division produces two standard systems for aerial refueling: 

  • Boom nozzle and receptacle system

  • Probe-and-drogue system

The boom nozzle and receptacle are the interface traditionally adapted for Air Force applications including strike aircraft, tankers and transports, while the probe-and-drogue are traditionally adapted for Navy/Marine strike aircraft and military trainers.

 

Staying on target non-stop

Elevating Flight with Decades Strong Aerial Refueling SolutionsAerial refueling is the process by which an aircraft is loaded with fuel mid-air while still in flight. The crucial operation allows military craft to fly prolonged maneuvers and reconnaissance missions. In some cases, our inflight refueling equipment has been incorporated into platforms derived from commercial aircraft. One noteworthy example is the Boeing 747-200 used for Air Force One.

 


Elevating Flight With Decades-Strong Aerial Refueling Solutions - C5 large transport refueling - Parker AerspaceParker’s development of in-flight refueling equipment began more than 55 years ago with Lockheed Martin’s reconnaissance aircraft, the SR71 Blackbird (1964). Parker designed the aerial refueling receptacle for this historic aircraft. After advancing early variants of a universal aerial refueling receptacle slipway installation (UARRSI) for the development of the Rockwell B-1 Lancer and the Fairchild A-10 Thunderbolt, Parker’s expertise was again put to use on the refueling receptacle for another U.S. fighter jet.  In those early days of evolving aerial refueling solutions, Parker augmented its knowledge base through the strategic acquisition of Schultz Tool and Manufacturing in 1971 a company that had designed receptacles for the F-111 Aardvark, the C-5 Galaxy, and the A-7 Corsair II.  


In 1997, Parker again advanced its air-to-air offerings and necessary ground test equipment by acquiring the aerial refueling product line from XAR Industries in California. The company had previously provided aerial refueling product designs for Lockheed Martin’s F-16, F-117, and F-22 as well as Universal Aerial Refueling Receptacle (UARRSI) variants.


Building on the technologies and applications from Parker, Shultz and XAR, our teams developed a unique receptacle and slipway assembly for the B-2 program. Since this time, Parker has subsequently designed multiple derivatives of the UARRSI and application-specific receptacles for several programs including the F-22 and F-35 programs.

 

Utah Air National Guard members from the 191st Air Refueling Squadron execute an air refueling mission from a KC-135 Stratotanker. A B-2 Spirit from the 509th Bomb Wing at Whiteman AFB, Missouri participated during this training mission. Video by Staff Sgt. Erin Mills.

 

The multi-purpose UARRSI convenience and adaptability

Elevating Flight With Decades-Strong Aerial Refueling Solutions - universal aerial refueling receptacle - Parker AerospaceIn 1976, Parker introduced an improved universal aerial refueling receptacle slipway installation (UARRSI) which has proven to be Parker’s most versatile piece of aerial refueling equipment. UARRSI adapts to aircraft that require a nozzle and receptacle-type apparatus. The unit features a lighted slipway and voice command functionality to facilitate the fuel transferring process. UARRSIs are used on military aircraft including the Boeing C-17, McDonnell Douglas KC-10, the Airbus A330 MRTT, and the Boeing GTTA, P-8A, and the 737 AEW&C E-7 Wedgetail. 

 


Testing equipment within critical industry standards

Elevating Flight With Decades-Strong Aerial Refueling Solutions - Aerial refueling testers - Parker AerospaceParker’s aerial refueling ground test kits are used to evaluate at the aircraft or component levels, along with the voice inter-communication capability. This testing function allows engineers to assess specific status modes (connect and disconnect), as well as alignment and engagement states of the equipment. Parker’s product line conforms to original equipment manufacturing (OEM) specifications, U.S. military standards, and additional requirements developed by the Aerial Refueling Systems Advisory Group (ARSAG) and other like agencies. 

 


Supporting the next generation of aerial refueling

Elevating Flight With Decades-Strong Aerial Refueling Solutions - next gen aerial refueling - Parker AerospaceThe future of in-flight refueling technology is now taking off in innovative directions, with a renewed emphasis on safety and efficiency. Aerial refueling for helicopters and unmanned aerial vehicles (UAVs) is also an active field of development. As the technology evolves, customers may see updated offerings from Parker based on our extensive pedigree, and our always-advancing capabilities. 

 

To learn more about the capabilities of Parker's Fluid Systems Division, please visit our website

This blog was contributed by the engineering team from the Fluid Systems Division of Parker Aerospace.

 

Related content

Defining Our Unique Contribution to the World

Reducing Lead Times by Half Earns Praise from Customer GA-ASI

Parker Aerospace Explores the Future of Aircraft Fuel Pumps

The History and Pedigree of Parker Aerospace Fluid Systems Division Fuel Pumps

Customizable Aircraft Fuel Pumps Reduce Cost and Boost Reliability

 

Follow Parker Aerospace on LinkedInFollow our Aerospace Technology page and learn more about Parker's products, technologies, and engineering solutions that are advancing the global aerospace fleet.

Have a question about Parker products or services? We can help: Contact Us!

Comments for Elevating Flight With Decades-Strong Aerial Refueling Solutions


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha