Sealing Shielding

QSFP-DD Optical Transceiver Thermal Interface Materials

QSFP-DD Optical Transceiver Thermal Interface Materials - QSFP-DD Overview - Parker ChomericsHigh performance QSFP-DD optical modules must use thermal interface materials to help dissipate heat efficiently and effectively to ensure the optimum operating performance, reliability and dependability of the high-speed transceiver.

The introduction of QSFP-DD, or Quad Small Form Factor Pluggable Double Density optical modules, have now doubled of the number of high-speed electrical interfaces that the module supports compared with a standard QSFP28 module.

Greater density, greater heat


QSFP-DD modules are the newest standard in high speed pluggable connectors, as they are the smallest form factor 400 G/s transceivers, offering the highest bandwidth density while leveraging the backward compatibility to lower-speed QSFP pluggable modules and cables. Highly integrated and advanced PAM-4 DSP chips, externally modulated laser (EML) diodes, and GaAs laser diodes enable the 400 G/s performance, yet these ICs come with significant thermal issues.

Power loads of up to 25W require significant considerations for heat dissipation, including the application of thermal interface materials.

The goal of a system thermal design is to remove the heat from the module case to ensure that the internal components in the module stay within operating temperature ranges to ensure optimal performance and reliability.

The role of thermal interface materials (TIMs)


Thermal interface materials such as thermally conductive gap filler pads, thermal greases, and dispensed thermal gels improve heat dissipation by filling minute air gaps and voids and by being dispensed or in contact with heat generating chipsets. Maximizing the contact area of the heatsink to the module lowers the thermal resistance and improves the system’s ability to cool the module. 

Types of TIMs available


High power thermal gels, such as Parker Chomerics THERM-A-GAP GEL 75, with 7.5 W/m-K thermal conductivity, as well as high performance single component thermal greases such as THERM-A-GAP GEL 8010 3 W/m-K, are typically robotically dispensed for high volume applications such as optical modules.
QSFP-DD Optical Transceiver Thermal Interface Materials - QSFP-DD Thermal Interface Materials - Parker Chomerics
Robotically dispensing thermal interface material can dramatically reduce costs, save valuable time, and greatly improve the overall performance of the QSFP-DD module. Thermal gap filler pads can be die cut into exact shapes to help dissipate heat from any heat generating component. Thermal gap filler pads provide a soft and effective method of heat dissipation as well as helping to reduce vibration stress for shock dampening. 

Need help deciding on a thermal interface material? Our recent blog Thermal Gels or Gap Filler Pads? Top 6 Things You Should Know can help!

Test

A TIM for every design; yes, even yours


Whatever your design is, be it a stacked card cage, or belly-to-belly, the thermal interface between the optical cable connector module and the heatsink attached to the outer case/cage is important to your design.

With speeds of 400 G/s being introduced now and 800 G/s on the near horizon, you must also consider the thermal heat dissipation needs of not only the module itself, but the interface connection on the PCB, as well as at the rack unit or cabinet level. 

Cabinets featuring 40U to 46U racks require immense thermal heat dispersion featuring both active and passive cooling technologies. Higher data transfer speeds, low latency, and constant availability require more computing power, which in turn means higher power densities per rack.

No matter what your thermal interface material need, Parker Chomerics can help, download our Thermal Interface Materials for Electronics Cooling Guide now!

 

QSFP-DD Optical Transceiver Thermal Interface Materials | Thermal Interface Materials Catalog | Parker Chomerics 

 

 

QSFP-DD Optical Transceiver Thermal Interface Materials | Jarrod Cohen | Parker Chomerics

This blog post was contributed by Jarrod Cohen, marketing communications for Parker Chomerics

 

 

 

 

 

 

 

Related Content:

How to Identify Quality Thermal Gap Fillers in Four Steps

Thermal Gels or Gap Filler Pads? Top 6 Things You Should Know

New THERM-A-GAP GEL 75 Thermal Gel Offers High Thermal Conductivity and Reliability

Have a question about Parker products or services? We can help: Contact Us!

Comments for QSFP-DD Optical Transceiver Thermal Interface Materials


Please note that, in an effort to combat spam, comments with hyperlinks will not be published.

Leave a comment





Captcha